2024-01-19 07:11 AM
The new STM32L4R9 svd file (version 2.0) has renamed
TIM1_OR2 to TIM1_AF1,
TIM1_OR3 to TIM1_AF2
Removed TIM1_OR1 which is in the reference manual containing ETR_ADC1_RMP and TI_RMP
Added a new TIM1_TISEL at offset 0x68 which is not in the current reference manual.
Is a new reference manual due and/or are these changes correct?
p.s. Thank you for fixing many of my previously reported issues and adding a lot of useful descriptions.
Regards, Kc
Solved! Go to Solution.
2024-01-19 08:50 AM - edited 2024-01-19 08:51 AM
Hello @Kevlar700 ,
Thank you for bringing the issue to our attention.
I reported this issue internally.
Internal ticket number: 171255 (This is an internal tracking number and is not accessible or usable by customers).
Thank you for your contribution in STCommunity 🙂.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-19 08:50 AM - edited 2024-01-19 08:51 AM
Hello @Kevlar700 ,
Thank you for bringing the issue to our attention.
I reported this issue internally.
Internal ticket number: 171255 (This is an internal tracking number and is not accessible or usable by customers).
Thank you for your contribution in STCommunity 🙂.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-19 09:00 AM - edited 2024-01-19 09:05 AM
Thank you.
The bit offsets in SDMMC_CLKCR are incorrect, which might make for a confusing debug session 🙂
2024-01-22 01:45 AM
Hello @Kevlar700 ,
Thank you for reporting this issue.
I reported internally.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.