Skip to main content
Nawres GHARBI
ST Technical Moderator
February 25, 2019
Question

STM32CubeMX 5.1.0 released

  • February 25, 2019
  • 30 replies
  • 7736 views

Dear community

We are pleased to announce the release of STM32CubeMX v5.1.0

What’s new ?

 

  • Performance enhancements for improved user experience.
  • Font size is now customizable (Click "Window" -> "Font size")
  • User interface updates
  • Graphics updates: TrueSTUDIO® is supported by TouchGFX Designer.

  • Added the support of the first MPU: STM32MP1 Series.
    • New devices: STM32MP151xx, STM32MP153xx, and STM32MP157xx.
    • New boards: STM32MP157A-EV1, STM32MP157C-EV1 and STM32MP157C-DK2
    • Features: Tj versus Ta calculation for PCC, DDR Test Suite, Device Tree generation, etc.
  • Added the support of the STM32WB Series:
  • New devices: STM32WB55xx.
    • Examples in MX format available in the STM32Cube_FW_WB_1.0.0 STM32CubeWB MCU Package.
    • Features: PCC Bluetooth® Low Energy feature.
  • Added the support of USBPD Middleware for G0 Series

Supported STM32Cube package versions:

·          STM32F0 V1.9.0

·          STM32F1 V1.7.0

·          STM32F2 V1.7.0

·          STM32F3 V1.10.0

·          STM32F4 V1.24.0

·          STM32F7 V1.15.0

·          STM32G0 V1.1.0

·          STM32H7 V1.3.2

·          STM32L0 V1.11.0

·          STM32L1 V1.8.1

·          STM32L4 V1.13.0

·          STM32MP1 V1.0.0

·          STM32WB V1.0.0

Main Fixed issues

 

  • 46874 [MX-Clock] include frac formulas in frequency calculation when PLL frac is enabled.
  • 51206 [MX-TIM] Break filter to be removed for TIM15, 16 and 17.
  • 53264 [MX-Pinout][STM32H750IBKx] G10 must be VSS and not VDD.
  • 55690 [MX-Board] Wrong configuration of special PHY reg for STM32F746 Discovery.
  • 56760 RCC for LTDC clock of STM32L4R9.
  • 56828 [MX-ETH]PHY DP83848 should support also RMII mode.
  • 56999 FreeRTOS™ initialization sequence.
  • 57348 [MX-LWIP] Exception generated due to undefined parameter in the ftl.
  • 57520 [MX-SPI] Missing Alternate Function Open Drain in SPI configuration mode.
  • 58043 [MX-TouchSensing] Missing user label in function MyTKeys_ErrorStateProcess().

Known limitations

Please read the Release note for the known limitations

https://www.st.com/resource/en/release_note/dm00107607.pdf

This topic has been closed for replies.

30 replies

Noppe.Jack
Senior
February 25, 2019

Hi Nawres,

Thank you for this update and for such a great tool in general. I have two quick questions:

  1. Curiosity: When do you think the update will be available for download?
  2. Serious: Where can I get more info on the issue & fix for the item "56999 FreeRTOS™ initialization sequence."

Nawres GHARBI
ST Technical Moderator
February 25, 2019

Hi @Noppe.Jack​ 

The update will be available very soon for download, just few hours for the website to synchronize

Concerning 56999 FreeRTOS™ initialization sequence, it has been fixed and will be available in the 5.1.0

Hope you enjoy the new release

Noppe.Jack
Senior
February 25, 2019

Thanks ... any info on what the original problem was? (I want to see if this relates to a problem I was having).

MNapi
Senior II
February 25, 2019

Hi I have been working lately with STM32L416KBU6

When I setup the clock in cube mx for example 50 MHz I get in Keil, which looks like half the speed 25 MHz. I wonder if there is a bug in Cube MX.

I noticed that he clocks are never accurate, I can never get like nice 1 MHz or 2 MHz. I wonder it is cheap low end board and you cannot expect too much.

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;

 RCC_OscInitStruct.MSIState = RCC_MSI_ON;

 RCC_OscInitStruct.MSICalibrationValue = 0;

 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;

 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;

 RCC_OscInitStruct.PLL.PLLM = 1;

 RCC_OscInitStruct.PLL.PLLN = 25;

 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;

 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

Nawres GHARBI
ST Technical Moderator
February 25, 2019

Hi @MNapi​ 

could you please create a separate ticket for this issue please

MNapi
Senior II
February 25, 2019

I could if I only knew where and how,

Nawres GHARBI
ST Technical Moderator
February 25, 2019

how did you measure the 25 MHz instead of the 50 MHz

MNapi
Senior II
February 25, 2019

When I setup PWM or OC clocks for example I did setup the main clock in Clube MX 50 Mhz

I used 50 divider to get 1 MHz instead I was getting something like 490 KHz. They were pretty close but never close. Like the main oscillator was not accurate.

When I did 25 divider I got like 990 KHz. I do have oscilloscope connected to the pins so I can see what is coming out.

I cannot see doing any mistake all looks simple and straightforward in Cube MX

But still if I do 50 MHz in Cube Mx shouldn't I get

RCC_OscInitStruct.PLL.PLLN = 50;

instead of

RCC_OscInitStruct.PLL.PLLN = 25;

Nawres GHARBI
ST Technical Moderator
February 26, 2019

could you please attach the used ioc

Dave Nadler
Senior III
February 25, 2019

@Nawres GHARBI​ How do we access the bug tracker where the details of the CubeMX fixed and outstanding issues are explained?

Nawres GHARBI
ST Technical Moderator
February 26, 2019

Hi @Dave Nadler​ 

The bug tracker isn't accessible for the moment but it is planned to be in the future

Dave Nadler
Senior III
February 25, 2019

@Nawres GHARBI​ It would be great if you would post these announcements AFTER the stuff is actually available on the web site (unless you intend to annoy your customers ;)

Nawres GHARBI
ST Technical Moderator
February 26, 2019

Hi @Dave Nadler​ 

The package was available on the web site when the post has been published, it may sometimes have a little late to appear to you depending on the web synchronization

anio1491
Associate II
February 25, 2019

Hello,

I was able to update my CubeMX (finally) to the release today (v5.1.0), but I am not able to update the L0 firmware package to the lastest version. I can see that there is a new packet available, but the download fails, and therefore, I cannot generate anymore code.

Any idea on what's wrong?

Please see screenshots attached.

Regards,

Andreea

0690X000006DpUMQA0.png

0690X000006DpURQA0.png

Nawres GHARBI
ST Technical Moderator
February 26, 2019

Hi @anio1491​ 

Trying to fix a server issue

Joerg Wagner
Senior III
February 25, 2019

Can we trust RC6 or should I wait for a final release?

Nawres GHARBI
ST Technical Moderator
February 26, 2019

Hi @Joerg Wagner​ 

The RC6 is the final release for 5.1.0

Joerg Wagner
Senior III
February 26, 2019

How to get rid of this message after generating code?

0690X000006DrRAQA0.png

Migrated a 5.0.1 project and never used GFXSIMULATOR in my life.

I find no appropiate config setting in the file <myproject>.ioc

There is no warning when building a new project from scratch.

Dave Nadler
Senior III
April 4, 2019

@Nawres GHARBI​ - Where is CubeMX plug-in 5.1? I'm trying to use this within Atollic.

I downloaded the software on this page: https://www.st.com/en/development-tools/stm32cubemx.html

Unfortunately that seems to be only the stand-alone executable, no plugin ZIP.

Thanks!

Dave Nadler
Senior III
April 4, 2019

@Nawres GHARBI​ - Running the stand-alone CubeMX (as plug-in is missing).

Try to generate code, says need to update repository, then fails to download (this bug reported before).

Unable to generate code now...

Help!

Thanks,

Best Regards, Dave

0690X0000089w5OQAQ.png