cancel
Showing results for 
Search instead for 
Did you mean: 

Issue in establishing FDCAN communication in Normal Mode

Shubh150
Associate III

I had sought help a while back for code on establish FDCAN communication in Classic mode between H7A3ZI-Q and G474RE, I did get the correct code and it indeed worked with the two boards, but now when I try to run it on Normal mode, the code fails to recieve data on the other end. It would be really helpful if someone explains how to do so. Please find attached zip files containg the code for FDCAN communication in Classic Mode.

1 REPLY 1
SofLit
ST Employee

Hello and sorry for the late answer.

I didn't understand the case. 

You said the following:


I did get the correct code and it indeed worked with the two boards, but now when I try to run it on Normal mode, the code fails to recieve data on the other end. 

The code worked on the two boards. What do you mean by that? in Loopback mode?

Check if you are using the correct FDCAN Tx/Rx pins connected to the transceivers i.e. the same as the ones configured in the CubeMx. 

For the pin config use HIGH or VERY_HIGH for pin speed.

 

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.