cancel
Showing results for 
Search instead for 
Did you mean: 

Interupt uart not working nucleo g431rb

NJP.1
Associate III

Hi all i am working in interrupt driven uart uart2 which is connected to the usb port in nucleo -g431rb The interrupt handler is not been called I have shared my code any thoughts kindly share.

void USART2_IRQHandler(void)
{
  /* USER CODE BEGIN USART2_IRQn 0 */
 
  uint32_t isrflags   = READ_REG(huart2.Instance->ISR);
  uint32_t cr1its     = READ_REG(huart2.Instance->CR1);
     if (((isrflags & USART_ISR_RXNE) != RESET) && ((cr1its & USART_CR1_RXNEIE) != RESET))
     {
         
         ch = huart2.Instance->RDR;
         
         HAL_UART_Transmit(&huart2, &ch, 1, 100);
     }
 
 
  /* USER CODE END USART2_IRQn 0 */
  HAL_UART_IRQHandler(&huart2);
  /* USER CODE BEGIN USART2_IRQn 1 */
 
  /* USER CODE END USART2_IRQn 1 */
}i
 
 
 
 
 
nt main(void)
{
  /* USER CODE BEGIN 1 */
 
  /* USER CODE END 1 */
 
  /* MCU Configuration--------------------------------------------------------*/
 
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
 
  /* USER CODE BEGIN Init */
 
  /* USER CODE END Init */
 
  /* Configure the system clock */
  SystemClock_Config();
 
  /* USER CODE BEGIN SysInit */
 
  /* USER CODE END SysInit */
 
  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_TIM1_Init();
  MX_TIM2_Init();
  MX_UART4_Init();
  MX_USART1_UART_Init();
  MX_USART2_UART_Init();
  MX_USART3_UART_Init();
  /* USER CODE BEGIN 2 */
 
  /* USER CODE END 2 */
 
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  uint8_t data[50] = "interupt uart testing\r\n";
  HAL_UART_Transmit (&huart2, data, sizeof (data), 100);
  while (1)
  {
	 // HAL_UART_Transmit (&huart1, data, sizeof (data), 10);
	  if(ch == 'a')
	  {
		  HAL_UART_Transmit (&huart2, data, sizeof (data), 100);
		  ch = 0;
	  }
	 // HAL_UART_Transmit (&huart3, data, sizeof (data), 10);
	 // HAL_UART_Transmit (&huart4, data, sizeof (data), 10);
    /* USER CODE END WHILE */
 
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
}

7 REPLIES 7
gbm
Lead III

Have you enabled the RXNE interrupt in UART and UART interrupt in NVIC?

HAL_UART interrupt routine will interfere with your interrupt handling. Maybe you should simply not cal it at all.

sizeof(data) is 50. The string should be defined as const char str [], then its size would be sizeof(str) - 1. ch variable must be volatile.

Piranha
Chief II

Think why the HAL has functions ending with ***_IT() and ***_DMA().

And learn splitting thoughts into sentences...

NJP.1
Associate III

Thankyou for the reply I got the solution I need to add the below line in the uart init funciton.

"USART2->CR1 |= (USART_CR1_TE | USART_CR1_RXNEIE | USART_CR1_RE | USART_CR1_UE);"

Thankyou for the reply..

Karl Yamashita
Lead II
  • You didn't enable UART Rx interrupt.
  • You should use HAL_UART_RxCpltCallback() when saving your data or setting a flag.
  • You need to keep track of HAL status for receive and transmit. Set an error flag for either one so you can test for !HAL_OK and either re-enable Rx interrupt or try and transmit again. I have snippets for the Rx as an example. For Tx, you'll have to figure out how to re-transmit data if HAL status returns HAL_BUSY.
  • Avoid transmitting from an interrupt. Instead save the data to a ring buffer and poll it. Then you can Transmit it from a polling routine.

int main(void)
{
  /* USER CODE BEGIN 1 */
 
  /* USER CODE END 1 */
 
  /* MCU Configuration--------------------------------------------------------*/
 
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
 
  /* USER CODE BEGIN Init */
 
  /* USER CODE END Init */
 
  /* Configure the system clock */
  SystemClock_Config();
 
  /* USER CODE BEGIN SysInit */
 
  /* USER CODE END SysInit */
 
  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_TIM1_Init();
  MX_TIM2_Init();
  MX_UART4_Init();
  MX_USART1_UART_Init();
  MX_USART2_UART_Init();
  MX_USART3_UART_Init();
  /* USER CODE BEGIN 2 */
 
  /* USER CODE END 2 */
 
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
    EnableUART_Interrupt();
  uint8_t data[50] = "interupt uart testing\r\n";
  HAL_UART_Transmit (&huart2, data, sizeof (data), 100);
  while (1)
  {
        if(GetUartEnErrorFlag())
        {
            ClearUartEnErrorFlag();
            EnableUART_Interrupt();
        }
 
	 // HAL_UART_Transmit (&huart1, data, sizeof (data), 10);
	  if(ch == 'a')
	  {
		  HAL_UART_Transmit (&huart2, data, sizeof (data), 100);
		  ch = 0;
	  }
	 // HAL_UART_Transmit (&huart3, data, sizeof (data), 10);
	 // HAL_UART_Transmit (&huart4, data, sizeof (data), 10);
    /* USER CODE END WHILE */
 
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
}
 
void EnableUART_Interrupt(void)
{
	if(HAL_UART_Receive_IT(&huart2, ch, 1) != HAL_OK)
	{
		UART_RxEnErrorFlag = true; // set error flag
	}
}
 
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
	if(huart->Instance == huart2.Instance) // check if UART2 caused interrupt
	{
		...// do something with data in ch variable. Typically save byte to a ring buffer for polling in main. Also ch holds the data already so no need to copy from DR register to ch variable.
		EnableUART_Interrupt(); // re-enable interrupt
	}
}
 
bool GetUartEnErrorFlag(void)
{
	return UART_RxEnErrorFlag;
}
 
void ClearUartEnErrorFlag(void)
{
	UART_RxEnErrorFlag = false;
}

I Can't Believe It's Not Butter. If you find my answers useful, click the accept button so that way others can see the solution.

Thankyou for the effort you have put I will implement the missed thing in my code. Thankyou..

Karl Yamashita
Lead II

Also for anyone wondering, when you call HAL_UART_Receive_IT(&huart2, ch, 1), you're telling HAL driver to save the incoming data to the ch variable. When HAL_UART_RxCpltCallback is called, ch holds the new data.

I Can't Believe It's Not Butter. If you find my answers useful, click the accept button so that way others can see the solution.