2025-03-18 9:21 PM - last edited on 2025-03-19 2:24 AM by mƎALLEm
Hi Everyone,
I interfaced Nucleo F767ZI with W25Q256JV using SPI and everything was working fine. But due to time and speed requirements, now I have to shift it to QSPI. I have used example code of STM Document named "QSPI_F769_discovery_flashloader" and developed a code for QSPI. But whenever I try to run the code and write/read the memory, nothing happens. I started to run code in debug on STMCube IDE and found that when try to send command to enable write and read status register, the register value doesn't change to write enable (0x02).
Always fail here and Error LED turns ON.
if (HAL_QSPI_AutoPolling(&hqspi, &sCommand, &sConfig, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK) {
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_7, GPIO_PIN_SET);
return QSPI_ERROR;
}
The Write Enable function is here.
uint8_t QSPI_WriteEnable(void) {
QSPI_CommandTypeDef sCommand;
QSPI_AutoPollingTypeDef sConfig;
memset(&sCommand, 0, sizeof(sCommand));
memset(&sConfig, 0, sizeof(sConfig));
/* Enable write operations ------------------------------------------ */
sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE;
sCommand.Instruction = WRITE_ENABLE_CMD;
sCommand.AddressMode = QSPI_ADDRESS_NONE;
sCommand.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
sCommand.DataMode = QSPI_DATA_NONE;
sCommand.DummyCycles = 0;
sCommand.DdrMode = QSPI_DDR_MODE_DISABLE;
sCommand.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
sCommand.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&hqspi, &sCommand, HAL_QPSI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK) {
return QSPI_ERROR;
}
/* Configure automatic polling mode to wait for write enabling ---- */
sConfig.Match = 0x02;
sConfig.Mask = 0x02;
sConfig.MatchMode = QSPI_MATCH_MODE_AND;
sConfig.StatusBytesSize = 1;
sConfig.Interval = 0x10;
sConfig.AutomaticStop = QSPI_AUTOMATIC_STOP_ENABLE;
sCommand.Instruction = READ_STATUS_REG_CMD;
sCommand.DataMode = QSPI_DATA_1_LINE;
if (HAL_QSPI_AutoPolling(&hqspi, &sCommand, &sConfig,
HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK) {
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_7, GPIO_PIN_SET);
return QSPI_ERROR;
}
return QSPI_OK;
}
Below is my attached qspi.h and qspi.c files and CubeMX configuration.
Kindly help me, what is the problem and if possible provide me a .c .h file for QSPI it's urgent.
Looking forward to suitable response, thanks in advance.
2025-03-18 10:12 PM - edited 2025-03-18 11:23 PM
hii @NajeebUllahKhan
Try following files ... there you may need to change flash size or other some parameters.
To test your quad spi is working or not take reference of following code
void testQSPI(){
QSPI_CommandTypeDef s_command;
uint8_t pData[3];
uint8_t wData[0x100];
uint8_t rData[0x100];
uint32_t i;
printf("***************QuadSPi Example*******************************\r\n");
BSP_QSPI_Init();
/*##-2-Read Device ID Test ###########################################*/
/* Read Manufacture/Device ID */
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = READ_ID_CMD;
s_command.AddressMode = QSPI_ADDRESS_1_LINE;
s_command.AddressSize = QSPI_ADDRESS_24_BITS;
s_command.Address = 0x000000;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
s_command.DataMode = QSPI_DATA_1_LINE;
s_command.DummyCycles = 0;
s_command.NbData = 2;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&hqspi, &s_command, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_QSPI_Receive(&hqspi, pData, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
printf("SPI I/0 Read Device ID : 0x%2X 0x%2X\r\n",pData[0],pData[1]);
/* Read Manufacture/Device ID Dual I/O*/
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = DUAL_READ_ID_CMD;
s_command.AddressMode = QSPI_ADDRESS_2_LINES;
s_command.AddressSize = QSPI_ADDRESS_24_BITS;
s_command.Address = 0x000000;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_2_LINES;
s_command.AlternateBytesSize= QSPI_ALTERNATE_BYTES_8_BITS;
s_command.AlternateBytes = 0;
s_command.DataMode = QSPI_DATA_2_LINES;
s_command.DummyCycles = 0;
s_command.NbData = 2;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&hqspi, &s_command, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_QSPI_Receive(&hqspi, pData, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
printf("Dual I/O Read Device ID : 0x%2X 0x%2X\r\n",pData[0],pData[1]);
/* Read Manufacture/Device ID Quad I/O*/
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = QUAD_READ_ID_CMD;
s_command.AddressMode = QSPI_ADDRESS_4_LINES;
s_command.AddressSize = QSPI_ADDRESS_24_BITS;
s_command.Address = 0x000000;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_4_LINES;
s_command.AlternateBytesSize= QSPI_ALTERNATE_BYTES_8_BITS;
s_command.AlternateBytes = 0x00;
s_command.DataMode = QSPI_DATA_4_LINES;
s_command.DummyCycles = 4;
s_command.NbData = 2;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&hqspi, &s_command, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_QSPI_Receive(&hqspi, pData, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
printf("Quad I/O Read Device ID : 0x%2X 0x%2X\r\n",pData[0],pData[1]);
/* Read JEDEC ID */
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = READ_JEDEC_ID_CMD;
s_command.AddressMode = QSPI_ADDRESS_NONE;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
s_command.DataMode = QSPI_DATA_1_LINE;
s_command.DummyCycles = 0;
s_command.NbData = 3;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&hqspi, &s_command, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_QSPI_Receive(&hqspi, pData, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
printf("Read JEDEC ID : 0x%2X 0x%2X 0x%2X\r\n\r\n",pData[0],pData[1],pData[2]);
/*##-3-QSPI Erase/Write/Read Test ###########################################*/
/* fill buffer */
for(i =0;i<0x100;i ++)
{
wData[i] = i;
rData[i] = 0;
}
if(BSP_QSPI_Erase_Block(0) == QSPI_OK)
printf(" QSPI Erase Block ok\r\n");
else
Error_Handler();
if(BSP_QSPI_Write(wData,0x00,0x100)== QSPI_OK)
printf(" QSPI Write ok\r\n");
else
Error_Handler();
if(BSP_QSPI_Read(rData,0x00,0x100)== QSPI_OK)
printf(" QSPI Read ok\r\n\r\n");
else
Error_Handler();
printf("QSPI Read Data : \r\n");
for(i =0;i<0x100;i++)
printf("0x%02X ",rData[i]);
printf("\r\n\r\n");
for(i =0;i<0x100;i++)
if(rData[i] != wData[i])printf("0x%02X 0x%02X ",wData[i],rData[i]);
printf("\r\n\r\n");
/* check date */
if(memcmp(wData,rData,0x100) == 0 )
printf(" W25Q128FV QuadSPI Test OK\r\n");
else
printf(" W25Q128FV QuadSPI Test False\r\n");
}
2025-03-19 1:41 AM
OK, let me check and I'll update my code accordingly and then will let you know.
Is the code you provided has tested before?
2025-03-19 2:18 AM - last edited on 2025-03-19 2:22 AM by mƎALLEm
I have tested it and made some changes but still not working. When I used the "void testQSPI()" function to check if QSPI is working, it is not working as "static uint8_t QSPI_AutoPollingMemReady(uint32_t Timeout)" this function give QSPI_ERROR on the line
if (HAL_QSPI_AutoPolling(&QSPIHandle, &s_command, &s_config, Timeout) != HAL_OK)
{
return QSPI_ERROR;
}
in QSPI_AutoPollingMemReady(uint32_t Timeout).
below is my attached updated files. and debug results.
Looking forward to your response...
2025-03-19 2:21 AM
Hello @NajeebUllahKhan,
Please use </> button to share your code.
See this post.
Thank you for your understanding.