cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-F767ZI + ADS1298 board - SPI communication issues

bog201
Associate II

Hi everyone,

I am having issues interfacing an ADS1298 board with a NUCLEO F767ZI. 

 

 

 

void ADS1298_ReadConfig1(SPI_HandleTypeDef *hspi) {
    uint8_t command[2] = {0x20 | 0x00, 0x00};  // RREG command for sending ID
    uint8_t sdatacCmd = 0x11; // SDATAC mode command for sending data

    GPIOA->BSRR = GPIO_BSRR_BR4; // CS LOW

    *(volatile uint8_t *)&SPI1->DR = sdatacCmd; // SDATAC command, stop reading data so the ADS1298 can receive commands -- direct register access method
	while (!(SPI1->SR & SPI_SR_TXE)); // Wait until TXE (Transmit buffer empty) is set
	while (SPI1->SR & SPI_SR_BSY);   // Wait for transmission to complete
	while (!(SPI1->SR & SPI_SR_RXNE)); // Wait until RXNE (Receive buffer empty) is set
	volatile uint8_t sdatac_status = *(volatile uint8_t *)&SPI1->DR; // Discard

	*(volatile  uint8_t *)&SPI1->DR = command[0];
	while (!(SPI1->SR & SPI_SR_TXE));
	while (SPI1->SR & SPI_SR_BSY); 
	while (!(SPI1->SR & SPI_SR_RXNE));
	volatile uint8_t rreg_status1 = *(volatile uint8_t *)&SPI1->DR; // Discard

	*(volatile uint8_t *)&SPI1->DR = command[1];
	while (!(SPI1->SR & SPI_SR_TXE)); 
	while (SPI1->SR & SPI_SR_BSY); 
	while (!(SPI1->SR & SPI_SR_RXNE));
	volatile uint8_t rreg_status2 = *(volatile uint8_t *)&SPI1->DR; // Discard

	*(volatile uint8_t *)&SPI1->DR = 0xFF; // Dummy byte
	while (!(SPI1->SR & SPI_SR_TXE)); 
	while (SPI1->SR & SPI_SR_BSY);
	while (!(SPI1->SR & SPI_SR_RXNE));
	response = *(volatile uint8_t *)&SPI1->DR; // Save ID in a buffer

	for ( int i = 0; i < 10; i++); // Small delay to have >2 us between last CLK falling edge and CS high
    GPIOA->BSRR = GPIO_BSRR_BS4; // CS HIGH
    printf("CONFIG1: 0x%02X\n", response);
}

 

 

DS1Z_QuickPrint7.png

I set DRDY (data ready pin) as an interrupt, meaning that this function runs every time DRDY toggles. It seems like I am getting the correct ID 0x92 at address 0x20 | 0x00, but for some reason I am also reading the CONFIG1 register 0x86 which is 0x20 | 0x01 at the beginning of each new SPI transaction. From the printf function I see CONFIG1: 0x86, even though it should be 0x92. 

 

I thought I am flushing the FIFO by reading the buffer each time I send a byte. Does anyone have any suggestions on what could cause the extra byte at the beginning of the SPI transactions? I also asked on the TI forums as it might be more ADS1298 related than the STM32 NUCLEO board.

0 REPLIES 0