2023-06-27 06:17 AM
Why does the STM32CubeIDE only allow selecting SPI1, SPI2 Full/Half Duplex slave mode for the STM32F072RBT6 Discovery board, while providing incorrect configuration options for Full duplex Master for SPI1, SPI2
Solved! Go to Solution.
2023-06-27 07:32 AM
Hello @Sudharshan and welcome to the Community 🙂,
Could you please check the "Parameter Settings" and precisely clock parameters-> prescaler (for baud rate).
Note that, the baud rate must be low or equal to 18 Mbit/s with 4 to 16 programmable bit frames.
Please let me know if the issue is solved.
Thank you .
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-06-27 07:32 AM
Hello @Sudharshan and welcome to the Community 🙂,
Could you please check the "Parameter Settings" and precisely clock parameters-> prescaler (for baud rate).
Note that, the baud rate must be low or equal to 18 Mbit/s with 4 to 16 programmable bit frames.
Please let me know if the issue is solved.
Thank you .
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-06-28 01:58 AM
Hello Kaouthar,
Thank you for your prompt response and providing the information regarding the "Parameter Settings" and clock parameters for the baud rate. I appreciate your assistance.
I have checked the parameters and made the necessary adjustments based on your instructions. The baud rate has been set to a value lower or equal to 18 Mbit/s, and I have ensured that the programmable bit frames are within the range of 4 to 16.
I will now test the system with these new settings to see if the issue is resolved. If I encounter any further difficulties or have any additional questions, I will reach out to you for further support.
Once again, thank you for your help.
Best regards,
Sudharshan
2023-06-30 02:32 AM
Hello @Sudharshan ,
If your first question has been answered, please close this topic by choosing Accept as Solution. This will help other users find that answer faster.
It is recommended to post a new question if you encounter any different difficulties or if you have any further questions.
Thank you for your contribution in the ST Community 🙂.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.