2020-06-12 5:20 PM
2020-06-12 8:30 PM
I suggest starting to read reference manual, because it explains it pretty clearly, but you didn't even care to write your MCU part number. You cannot do 32-bit writes to 16-bit register, therefore the correct answer is the second one - two 16-bit writes.
If your MCU has it, SAI peripheral is preferred for audio protocols.
2020-06-12 11:55 PM
If this is the two-port DMA, the memory-side alignment requirement is given by the DMA itself, if the FIFO is used (i.e. not in direct mode). Read the DMA chapter in RM.
JW