cancel
Showing results for 
Search instead for 
Did you mean: 

I AM GETTING THIS TYPE OF ERROR

Kband.1
Associate II

I AM USING STMf030c6

1 ACCEPTED SOLUTION

Accepted Solutions
Andrew Neil
Evangelist III

You need to pay attention to what it's telling you in the 'Build Output' window:

0693W000008xNvpQAE.jpgNote that you can copy & paste the text from that window - which is often more useful than a screenshot.

So your Flash Algorithm is not correctly configured; this is part of the Debug configuration in the Project options - though it should have been automatically set by the target chip selection

View solution in original post

4 REPLIES 4

In project options go to debug settings and under the flash settings add in the STM32 part you are using.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Evangelist III

You need to pay attention to what it's telling you in the 'Build Output' window:

0693W000008xNvpQAE.jpgNote that you can copy & paste the text from that window - which is often more useful than a screenshot.

So your Flash Algorithm is not correctly configured; this is part of the Debug configuration in the Project options - though it should have been automatically set by the target chip selection

tq neil

You're welcome

0693W000008ww08QAA.png