How to call timer interrupt using registers? [NO HAL DRIVERS]
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-12 9:50 AM
Hi, i am trying to call timer interrupt handler using registers and the following is my code, but the problem is that the function is being not called, I see no output in the oscilloscope or live expression. First my DAC value is still 0, the counter is running though. I also tried to use toggle breakpoint to see where the problem lies and I think it's at this point // Clear the interrupt flag
TIM2->SR &= ~TIM_SR_UIF;
but i am not sure. Could anyone confirm if what i am doing is correct/wrong?
Btw, i am using stm32-g071rb.
int main(){
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_DAC1_Init();
MX_TIM2_Init();
/* USER CODE BEGIN 2 */
// TIM2->DIER |= TIM_DIER_UIE; // Enable the update (overflow) interrupt
NVIC_SetPriority(TIM2_IRQn, 0); // Set the interrupt priority (if needed)}
NVIC_EnableIRQ(TIM2_IRQn); // Enable the timer interrupt in the NVIC
TIM2->CR1 |= TIM_CR1_CEN; // Start the timer
}
void TIM2_IRQHandler(void)
{
/* USER CODE BEGIN TIM2_IRQn 0 */
if (TIM2->SR & TIM_SR_UIF)
{
// Timer interrupt flag is set, do something here
DAC1->DHR12L2 = 1;
HAL_Delay(100);
//
// Clear the interrupt flag
TIM2->SR &= ~TIM_SR_UIF;
}
/* USER CODE END TIM2_IRQn 0 */
HAL_TIM_IRQHandler(&htim2);
/* USER CODE BEGIN TIM2_IRQn 1 */
/* USER CODE END TIM2_IRQn 1 */
}
Solved! Go to Solution.
- Labels:
-
Interrupt
-
STM32G0 Series
-
TIM
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-13 1:32 AM
The first problem is the use of HAL_Delay in the ISR. This call wiiil never return, as it is waiting for a lower priority interrupt to occur while called from a higher priority interrupt. This will not work.
Other problems: you cllear the interrupt flag incorrectly, using &= instead of a simple assignment =. You don't need to call HAL_TIM_IRQHandler() from your routine, it doesn't make sense.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-12 12:24 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-12 1:21 PM
And also this:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-12 2:29 PM
Your code looks good, Here is my code (for the STM32L010) that works perfectly. Th only comment I have on your code is why did you comment out the line // TIM2->DIER |= TIM_DIER_UIE; This is needed to set the Timer to interrupt. This may have been set already if you checked the interrupt checkbox in the HAL Timeer setup dialog
void SysTick_Init(void)
{
#ifdef BARE_METAL
SET_AND_WAIT(RCC->APB2ENR, RCC_APB2ENR_TIM21EN); /* Enable TIM21 Clock */
TIM21->PSC = 3; /* divide by 4 prescaler */
TIM21->ARR = 5242; /* set the countdown value */
#endif
TIM21->DIER |= TIM_DIER_UIE; /* Enable the interrupt */
TIM21->CR1 |= TIM_CR1_CEN; /* Enable the timer */
NVIC_EnableIRQ( TIM21_IRQn );
}
void TIM21_IRQHandler(void)
{
if (TIM21->SR & TIM_SR_UIF)
{
SysTick_Milliseconds += TICK_PERIOD_IN_MS;
}
TIM21->SR = 0; /* Clear all interrupts */
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-12 4:08 PM
You have a race condition here. You should only clear the flag if UIF is set. Otherwise you may clear it without it being handled.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-13 1:14 AM
Yes, the tim2 is checked mark in the CubeMx as a global interrupt already that's why I commented that part in the code.
But I see when the timer interrupt is enabled, my CNT is always at 0. Why is that so?
PS: Nevermind, it worked now.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-13 1:32 AM
The first problem is the use of HAL_Delay in the ISR. This call wiiil never return, as it is waiting for a lower priority interrupt to occur while called from a higher priority interrupt. This will not work.
Other problems: you cllear the interrupt flag incorrectly, using &= instead of a simple assignment =. You don't need to call HAL_TIM_IRQHandler() from your routine, it doesn't make sense.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-13 1:43 AM
I just turned off the interrupt in cubemx and called it manually in the code so now the HAL_TIM_IRQHandler() is not there anymore. Now, my value is changing. Thanks :)