cancel
Showing results for 
Search instead for 
Did you mean: 

Hi ST,Do you have any updates on MCU board to support I3C?Thank you,

hlee.3
Associate
 
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @hlee.3​, to the community!

STM32 with I3C interface will be available soon, look forward to it now!

Stay tuned and check the newsroom from time to time!

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Welcome, @hlee.3​, to the community!

STM32 with I3C interface will be available soon, look forward to it now!

Stay tuned and check the newsroom from time to time!

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Amel NASRI
ST Employee

Another option: Worldwide webcast: STM32 Innovation Live - STMicroelectronics

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Uwe Bonnes
Principal III

I subscribed to the webcast several time with several addresses and I never got an invitation back.