cancel
Showing results for 
Search instead for 
Did you mean: 

Is it coming official update of SBSFU to support CubeMX?

YUTA1
Associate II

Hello everyone,

Now I'm developing an user application compatible with SBSFU on STM32CubeIDE.

SBSFU itself is pretty nice, but I feel the development architecture and environment are a little bit old, like not supporting CubeMX.

Fortunatelly, I succeeded to work my user application, that is developed on Visual Studio Code (with CubeMX and STM32 VSCode Extension), with SBSFU.

However, it's hard challenge for me to more update like below, because I'm beginenr for embedded system.

  • call some functions located in SE interface region from the user application developped with the above environment
  • change the communication protocol from YMODEM to other ones in SBSFU (this SBSFU means the STM32 project of bootloader, not whole package)

I appreciate if the official update of SBSFU will be coming to support the moden development environment kinds of CubeMX and Visual Studio Code. 

Within a few years ago, there're several users who has similar requirements of this matter. 

But there's less infromation in recent years.  

Does anyone know the recent activities or future plan about this?

Thank you for your help in advance!

1 ACCEPTED SOLUTION

Accepted Solutions
Jocelyn RICARD
ST Employee

Hello @YUTA1 ,

The X-CUBE-SBSFU package is still in maintenance even if it was not updated for long.

A new release should come soon fixing issues and updating drivers.

Unfortunately there is no short term plan to have a direct compatibility between a project generated by CubeMX and the SBSFU.

On recent STM32H5, a so called boot path feature was added to CubeMX to be able to address this, but it will not be deployed because it is far too heavy to maintain.

Regarding the call to function located in SE_Interface, you just need to copy paste what already exists.

There is no specific documentation for this.

Regarding the change of Ymodem protocol by another protocol many customers do this without any issue.

The SBSFU package goal is to provide a secure boot and secure firmware implementation example that addresses most of STM32 families (except the one based on CM33 actually).

It is generic enough to allow adaptation to any environment and constraints.

Just in case, there are 2 useful documents: The User manual UM2262 and the Integration guide AN5056.

Best regards

Jocelyn

 

View solution in original post

4 REPLIES 4
Jocelyn RICARD
ST Employee

Hello @YUTA1 ,

The X-CUBE-SBSFU package is still in maintenance even if it was not updated for long.

A new release should come soon fixing issues and updating drivers.

Unfortunately there is no short term plan to have a direct compatibility between a project generated by CubeMX and the SBSFU.

On recent STM32H5, a so called boot path feature was added to CubeMX to be able to address this, but it will not be deployed because it is far too heavy to maintain.

Regarding the call to function located in SE_Interface, you just need to copy paste what already exists.

There is no specific documentation for this.

Regarding the change of Ymodem protocol by another protocol many customers do this without any issue.

The SBSFU package goal is to provide a secure boot and secure firmware implementation example that addresses most of STM32 families (except the one based on CM33 actually).

It is generic enough to allow adaptation to any environment and constraints.

Just in case, there are 2 useful documents: The User manual UM2262 and the Integration guide AN5056.

Best regards

Jocelyn

 

opcode
Associate

I apologize for hijacking this thread but would appreciate if you could add some more clarification on the following point:

On recent STM32H5, a so called boot path feature was added to CubeMX to be able to address this, but it will not be deployed because it is far too heavy to maintain.

I am investigating the feasibility of implementing a glue layer between CubeMX and SBSFU to help with a large development project we are planning internally. It seems to be a significant effort but feasible. However, in your response, you define the maintenance effort as 'far too heavy'.

So obviously, I am missing something in my assessment of the required work.

Are there any specific fundamental features missing that make integration between CubeMX and SBSFU unexpectedly difficulty? Or is the development of CubeMX so rapid and shifting that maintaining SBSFU compatibility would require constant effort?

Again, not questioning your assessment, just trying to save myself unexpected pain from unforeseen issues.

Thank you in advance for your response.

YUTA1
Associate II

@Jocelyn RICARD -san, 
Thank you for your quick response, and I apologize for late reply.
I understood that there wouldn't be no official update of compatibility with CubeMX project structure in the near future.

I'll try to work on migrating the architecture by myself.
Thank you for your kindness.

Hello @opcode ,

I'm sorry, I was not clear enough. I was talking about the maintenance of CubeMX's boot path feature only.

There is no issue using CubeMX to generate your application's project and make the few adaptations needed to be mapped in active slot of SBSFU.

Best regards

Jocelyn