2024-07-04 08:28 AM
I need to generate a pulse which is activated high immediately by rising/falling input signal around 100Hz with varied width. I have tried One Pulse Mode and Gated Mode on STM32f334R8T6 so far but none of them were successful. Even I tried on HRTIM, but I did not get how to generate a pulse with determined width after receiving an event.
The image below shows the problem. I appreciate any help in this regard.