I'm not sure that the counter waveform (on which we see blue and purple marks) are showing the exact behavior of the timer counter. First, the CMP > 3 is indeed the requirement, but the CMP=0 is also a valid usecase: "Null duty cycle exception case" ...
Dear User, Based on information you provided, I think that such behavior is indeed what is expected by the programming: When current shift is less than 50%, and a new shift programming occurs, if the preload option is not applied, and the counter of ...
Hello, I understand your need to go down till 100Hz, but the lowest frequency allowed by the STM32CubeMx configuration is 384Hz for Hrtim. Allowing such low frequency is not a common use case with STM32CubeMx, so I'm not sure that such modification w...
Hello, Yes, this sounds correct, if the computation of SET/RESET events could be done fast enough regarding the PWM period.Please, notice that enabling the preload of registers is a good practice, allowing the update to be taken in next update event ...
Hello, In order to synchronize all PWM, Master timer period (or compares in master timer unit) could be used as a reset source for other timer unit. This will ensure all timers roll-over at the same moment. Make sure also please to enable all Timer u...