cancel
Showing results for 
Search instead for 
Did you mean: 

forum displaying posts out of order

trevor23
Associate III
Posted on June 21, 2010 at 17:29

forum displaying posts out of order

#falt-view
11 REPLIES 11
Andrew Neil
Evangelist III
Posted on May 17, 2011 at 13:55

''Are others seeing posts out of order?''

Yes, I have been seeing that for a week or two.

For me, the workaround seems to be to switch from ''flat'' to ''Threaded'' mode.

FWIW, I think this forum software is dreadful.

trevor23
Associate III
Posted on May 17, 2011 at 13:55

Agreed, but what makes it more frustrating is that the old forum worked very well

t1
Associate II
Posted on May 17, 2011 at 13:55

''FWIW, I think this forum software is dreadful.''

Agreed, although I've seen a lot worse.

picguy2
Associate II
Posted on May 17, 2011 at 13:55

Forum s/w should default or at least remember thread view.  Larger font size would help.  Also not going to top after reading a post halfway down.

Andrew Neil
Evangelist III
Posted on May 17, 2011 at 13:55

It does!

Doesn't look like anyone's going to own-up to what went wrong, or say what had to be done to fix it, though...

trevor23
Associate III
Posted on May 17, 2011 at 13:55

seems to be working correctly again

PeppeST
ST Employee
Posted on May 17, 2011 at 13:55

Hi ,

the correct Flat View sorting configuration setup has been put back.

So, it should be OK now.

Ciao

Peppe

trevor23
Associate III
Posted on May 17, 2011 at 13:55

Great, thanks for the explanation

t1
Associate II
Posted on May 17, 2011 at 13:55

Doesn't seem to be fixed completely.  The topic

''Code causes hard fault, can anyone guess why'' is still out of order for me.