2010-06-21 08:29 AM
forum displaying posts out of order
#falt-view2011-05-17 04:55 AM
''Are others seeing posts out of order?''
Yes, I have been seeing that for a week or two. For me, the workaround seems to be to switch from ''flat'' to ''Threaded'' mode. FWIW, I think this forum software is dreadful.2011-05-17 04:55 AM
Agreed, but what makes it more frustrating is that the old forum worked very well
2011-05-17 04:55 AM
''FWIW, I think this forum software is dreadful.''
Agreed, although I've seen a lot worse.2011-05-17 04:55 AM
Forum s/w should default or at least remember thread view. Larger font size would help. Also not going to top after reading a post halfway down.
2011-05-17 04:55 AM
It does!
Doesn't look like anyone's going to own-up to what went wrong, or say what had to be done to fix it, though...2011-05-17 04:55 AM
seems to be working correctly again
2011-05-17 04:55 AM
Hi ,
the correct Flat View sorting configuration setup has been put back. So, it should be OK now. Ciao Peppe2011-05-17 04:55 AM
Great, thanks for the explanation
2011-05-17 04:55 AM
Doesn't seem to be fixed completely. The topic
''Code causes hard fault, can anyone guess why'' is still out of order for me.