cancel
Showing results for 
Search instead for 
Did you mean: 

FDCAN communication issue with STM32H743ZI Nucleo board

DJ_IND
Associate III

Hi,

I am using STM32H743 nucleo board on one of my design. On my board I have installed nucleo board on board to board connector. For FDCAN interface we are using TCAN3414 transceiver IC. Our bit rate is 1MHz and data rate 2MHz for FDCAN communication on board. We are interfacing the FDCAN with DigiSoM board having transceiver TMC2517. After some packet transmission i observed that communication link is down. CAN bus is not working. On resetting the controller communication starts again for sometime and again stops. I tried replacing the STM32H753 board with STM32H743 and i have not observed any communication issue on that particular system. On other system I am already having STM32H753 but still I am facing the same issue. I am using normal wires for GND CANH and CANL connections of length 15cm max. I tried reducing the baud rate till 250kbps but same issue. I have checked the signal quality on oscilloscope which looks fine with ringing effects. We are using MATLAB modelling for all this testing. Below is the cubeMX setting we are using for FDCAN1/2. Can you please help me what may be the issue here. Because on some nucleo boards with STM32H753ZI i have not seen any issue.

DJ_IND_0-1751294920099.png

DJ_IND_1-1751294965389.png

 

 

10 REPLIES 10

Can't see your FDCAN clock value.

Upload your IOC file for the STM32 that is working. And also the IOC file for the STM32 that is not working  

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source