cancel
Showing results for 
Search instead for 
Did you mean: 

FDCAN bootloader on UFBGA169 STM32H743AI

DrDro
Associate III

Hi,

App note AN2606 says I should use FDCAN1_Rx pin PH14 (similary Tx pin) to be able to use FDCAN bootloader but selected package UFBGA169 doesn't have such pins.

Can I use default FDCAN Pins to work with bootloader?

1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hello @DrDro ,

A similar question is already asked here.

For STM32H743, you can activate the FDCAN bootloader with only by PH13/PH14 pins.

When your question is answered, please close this topic by choosing "Accept as Solution". This will help other users find that answer faster.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
KDJEM.1
ST Employee

Hello @DrDro ,

A similar question is already asked here.

For STM32H743, you can activate the FDCAN bootloader with only by PH13/PH14 pins.

When your question is answered, please close this topic by choosing "Accept as Solution". This will help other users find that answer faster.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

What does that mean "you can activate the FDCAN bootloader with only by PH13/PH14 pins."?

Those pins dont exist right?

we dont need to firmware by ourselves, lets talk
KDJEM.1
ST Employee

Hello @Javier1

As mentioned in AN2606, for STM32H74, the FDCAN bootloader pins are PH13 and PH14. So, if the PH13 and PH14 pins are not available in some packages, the FDCAN bootloader is not supported. 

KDJEM1_2-1737032045459.png

The LQFP100, TFBGA100, LQFP144, and UFBGA169 STM32H743 packages do not have PH13 and PH14 pins, so the FDCAN bootloader is not supported.

KDJEM1_1-1737031998208.png

Thank you.

Kaouthar

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


@KDJEM.1 wrote:

if the PH13 and PH14 pins are not available in such packages, the FDCAN bootloader is not supported. 


That's really not very clear at all!

See: 

https://community.st.com/t5/stm32-mcus-products/fdcan-rom-bootloader-pins-for-stm32h743zi/td-p/762439

And:

https://community.st.com/t5/stm32-mcus-embedded-software/fdcan-bootloader-for-stm32h750vb/td-p/95844

 

The document needs to be updated to make this clearer.

KDJEM.1
ST Employee

Hello, 

 

Thank you @Andrew Neil and @Javier1 for reporting your feedback about the AN2606 application note. I reported internally your suggestion to add a note “Where these pins are available” to clarify the behavior this discussion FDCAN ROM bootloader pins for stm32H743ZI - STMicroelectronics Community.

Note that, also I reported internally the datasheet typo for correction.

KDJEM1_0-1737033807096.png

 

Thank you for your contribution in STCommunity.

Internal ticket number: 200567  (This is an internal tracking number and is not accessible or usable by customers). 

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.