2021-05-12 3:14 PM
I started getting this message when I try to debug my code. However, there are currently no breakpoints in my code at all. I have gotten this in the past and I deleted and redownloaded the IDE which I really do not want to do again. I am running it on Mac. Any suggestions are helpful.
// Simple ADC Reader
// ADC1_1 on PA1
// Port A on AHB1
// ADC on APB2
#include "stm32f4xx.h"
#include "printUSART.h"
int val = 0;
int main(void){
USART2_Init();
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOAEN;
GPIOA->MODER = GPIO_MODER_MODE0_0 | GPIO_MODER_MODE0_1;
RCC->APB2ENR |= RCC_APB2ENR_ADC1EN;
ADC1->CR2 = 0;
ADC1->SQR3 |= ADC_SQR3_SQ1_0;
ADC1->CR2 |= ADC_CR2_ADON;
while(1){
ADC1->CR2 |= ADC_CR2_SWSTART;
while(!(ADC1->SR & ADC_SR_EOC)){}
val = ADC1->DR;
printf("\n%d", val);
}
}
2021-05-12 4:44 PM
I don't Cube/Eclipse.
JW
2021-05-13 2:18 AM
I get this error in cubeIDE when indeed i add more than 6 breakout points.
I can resume normal debugging when i remove breakout points down to 6
2021-05-13 2:22 PM
That would make sense except I don’t have any breakpoints at all in my code...
2021-05-18 8:02 AM
do you have more than one project opened in stm32ide workspace?
maybe youre trying to debugg the wrong code?
2024-07-14 8:59 AM - edited 2024-07-14 9:01 AM
Encountered today the same problem today - no breakpoints in the breakpoint view, used brk / del debugger commands to delete all breakpoints but still no luck.
Eventually figured out that the function, where I wanted to put the breakpoint in, was likely optimised to inline and the IDE was actually trying to insert multiple breakpoints instead of one - and I only had 3 HW breakpoints available in the MCU.
If that is the case need to disable optimisation or find another way/place to insert the breakpoint.