cancel
Showing results for 
Search instead for 
Did you mean: 

Help needed in "STM32(OpenOCD)" Debuging with STM32F030f4x MCU

Kai_Satone
Senior

Open On-Chip Debugger 0.12.0-00024-gc3ff39f8b (2023-06-26-16:51) [https://github.com/STMicroelectronics/OpenOCD]

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : connected to stlink-server

Info : stlink-server API v3, version 2.1.1

Info : STLINK V2J43S7 (API v2) VID:PID 0483:3748

Info : Target voltage: 3.304021

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

Info : clock speed 4000 kHz

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x0bb11477

Info : [STM32F030F4Px.cpu] Cortex-M0 r0p0 processor detected

Info : [STM32F030F4Px.cpu] target has 4 breakpoints, 2 watchpoints

Info : starting gdb server for STM32F030F4Px.cpu on 3333

Info : Listening on port 3333 for gdb connections

Error: [STM32F030F4Px.cpu] clearing lockup after double fault

Polling target STM32F030F4Px.cpu failed, trying to reexamine

Info : [STM32F030F4Px.cpu] Cortex-M0 r0p0 processor detected

Info : [STM32F030F4Px.cpu] target has 4 breakpoints, 2 watchpoints

Info : accepting 'gdb' connection on tcp/3333

Info : device id = 0x10006444

Info : flash size = 32 KiB

shutdown command invoked

Info : dropped 'gdb' connection

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0