cancel
Showing results for 
Search instead for 
Did you mean: 

Enabling instruction prefetch in the HAL (potential bug)

GG.2
Associate II

Hello,

According to the reference manual RM0456 7.3.3:

"Prefetch is enabled by setting PRFTEN in FLASH_ACR.
PRFTEN must be set only if at least one wait state is needed to access the flash memory"

 

Compared to that I've seen that in the U5 HAL, in the function HAL_Init() there is a call to `__HAL_FLASH_PREFETCH_BUFFER_ENABLE()` (when `PREFETCH_ENABLE` is defined).

This means that prefetch might be enabled even when there are 0 wait states to access flash memory (because this is not enforced), contradicting what the reference manual says.

 

Is it intentional? or might cause undefined behavior?

Thank you

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

Hello,

That' true the macro is called in the HAL: 

HAL_StatusTypeDef HAL_Init(void)
{
/* Configure Flash prefetch */
#if (PREFETCH_ENABLE != 0U)
__HAL_FLASH_PREFETCH_BUFFER_ENABLE();
#endif /* PREFETCH_ENABLE */

But the software flag is activated in the example itself in stm32u5xx_hal_conf.h file:

#define PREFETCH_ENABLE 1U /*!< Enable prefetch */

stm32u5xx_hal_conf.h file is not part of the HAL but part of your example or project.

So you need to set it to 0 in your case.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

5 REPLIES 5

Probably less consequential if the Flash can service with no delay, but yes language here seems awkward and could.be explained more clearly and reasoned. @Sarra.S 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Sarra.S
ST Employee

Hello @GG.2@Tesla DeLorean

Thank you for bringing this question to my attention! 

>>This means that prefetch might be enabled even when there are 0 wait states to access flash memory 

This case is not applicable in U5 Flash examples, in fact, all the examples run at 160MHz, according to this frequency, there are 4 wait states (Check RM) : 

SarraS_1-1697451396583.png

So prefetch has to be enabled, and PRFTEN must be set since there is more than 1 wait state needed. 

I hope this is much more clear.  

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

The problem is that I'm running my own code, not the examples, and the HAL should not assume the HCLK frequency... In my case I run at 12MHZ range 4 with 0 WS

Hello,

That' true the macro is called in the HAL: 

HAL_StatusTypeDef HAL_Init(void)
{
/* Configure Flash prefetch */
#if (PREFETCH_ENABLE != 0U)
__HAL_FLASH_PREFETCH_BUFFER_ENABLE();
#endif /* PREFETCH_ENABLE */

But the software flag is activated in the example itself in stm32u5xx_hal_conf.h file:

#define PREFETCH_ENABLE 1U /*!< Enable prefetch */

stm32u5xx_hal_conf.h file is not part of the HAL but part of your example or project.

So you need to set it to 0 in your case.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

No, I think the question relates to the 0 WS line, and how exactly the FLASH and Prefetch pathing is working, or required to work.

I think a white paper illustrating some of the plumbing, clocking and core connectivity would help show what needs to be enabled, or not, and why, as it relates to reads of memory, and data flows.

SarraS_2-1697451396583.png

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..