cancel
Showing results for 
Search instead for 
Did you mean: 

Changing address for UART Character match does not work as specified

Uwe Bonnes
Principal III

E.g. RM0351 Rev 6 tells for UART/CR2 / ADDR:

" This bit field can only be written when reception is disabled (RE = 0) or the USART is disabled (UE=0)"

However it seems thaT RE = 0 is not sufficient. Only with UE = 0, a new address may be written.

(gdb) p /x USART1->CR1 = 0x401c

$32 = 0x401c

(gdb) p /x USART1->CR2 = 0x13000000

$33 = 0x13000000

(gdb) p /x USART1->CR2

$34 = 0x13000000

(gdb) p /x USART1->CR1 = 0x4019

$35 = 0x4019

(gdb) p /x USART1->CR2 = 0x11000000

$36 = 0x11000000

(gdb) p /x USART1->CR2

$37 = 0x13000000

Do I do something wrong or is this an undocumented error?

0 REPLIES 0