cancel
Showing results for 
Search instead for 
Did you mean: 

CAN start API not executing in stm32F446RE board

Komal
Associate II

Hi ST,

Can you please suggest me the solution of my problem, below is the problem statement

I have configured the stm32f446RE oard to use CAN1 in loopback mode, using CAN start in a function but the MSR bit 0 INAK is not resetting in the HAL_CAN_Start API

please find my code in the attachment 
i am use 500kbps baudrate.

Hoping for your quick response.

Note: Tried by increasing the CAN_TIMEOUT_VALUE but the CAN_Sart is not coming out of the while loop

 

/* Wait the acknowledge */
while ((hcan->Instance->MSR & CAN_MSR_INAK) != 0U)
{
/* Check for the Timeout */
if ((HAL_GetTick() - tickstart) > CAN_TIMEOUT_VALUE)

 





Requesting for fast response 

1 ACCEPTED SOLUTION

Accepted Solutions

Hello,

I've already looked at your code from your attached main and you are using LoopBack mode.

So please review my answer in my previous comment:

  1. - You need to set new values for BS1, BS2 and CAN prescaler: see this thread: https://community.st.com/t5/stm32-mcus-products/can1-loopback-does-not-work-on-stm32f427/m-p/695622
  2. - You need to set the internal pull-up for CAN_Rx pin.

The code you shared don't give a full picture of all your configuration. You need to share your project including the ioc file.

EDIT: updated the correct link to the thread.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
mƎALLEm
ST Employee

Hello,

First, please use </> button to paste your code. Read our recommendations on this link: https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

Second, did you enable the internal pull-up resistor on CAN-RX pin?

Also see these parameters are bad:

 

 

  hcan1.Init.Prescaler = 6;
  hcan1.Init.TimeSeg1 = CAN_BS1_11TQ;
  hcan1.Init.TimeSeg2 = CAN_BS2_2TQ;

 

 

 See this thread: https://community.st.com/t5/stm32-mcus-products/can1-loopback-does-not-work-on-stm32f427/m-p/695622

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

please find the code 

/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * Copyright (c) 2023 STMicroelectronics.
  * All rights reserved.
  *
  * This software is licensed under terms that can be found in the LICENSE file
  * in the root directory of this software component.
  * If no LICENSE file comes with this software, it is provided AS-IS.
  *
  ******************************************************************************
  */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
 CAN_HandleTypeDef hcan1;

/* USER CODE BEGIN PV */
 CAN_TxHeaderTypeDef   TxHeader;
 CAN_RxHeaderTypeDef   RxHeader;
 uint8_t               TxData[8];
 uint8_t               RxData[8];
 uint32_t              TxMailbox;
 uint8_t			   test;
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_CAN1_Init(void);
/* USER CODE BEGIN PFP */
static HAL_StatusTypeDef CAN_Polling(void);
/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{
  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_CAN1_Init();
  /* USER CODE BEGIN 2 */

  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
	  if(CAN_Polling() == HAL_OK)
	   {
	 	  test=1;
	   }
	   else
	   {
	 	  test=2;
	   }

  }
  /* USER CODE END 3 */
}

/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  /** Configure the main internal regulator output voltage
  */
  __HAL_RCC_PWR_CLK_ENABLE();
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
  RCC_OscInitStruct.PLL.PLLM = 16;
  RCC_OscInitStruct.PLL.PLLN = 336;
  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
  RCC_OscInitStruct.PLL.PLLQ = 2;
  RCC_OscInitStruct.PLL.PLLR = 2;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
  {
    Error_Handler();
  }
}

/**
  * @brief CAN1 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_CAN1_Init(void)
{

  /* USER CODE BEGIN CAN1_Init 0 */

  /* USER CODE END CAN1_Init 0 */

  /* USER CODE BEGIN CAN1_Init 1 */

  /* USER CODE END CAN1_Init 1 */
  hcan1.Instance = CAN1;
  hcan1.Init.Prescaler = 6;
  hcan1.Init.Mode = CAN_MODE_LOOPBACK;
  hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
  hcan1.Init.TimeSeg1 = CAN_BS1_11TQ;
  hcan1.Init.TimeSeg2 = CAN_BS2_2TQ;
  hcan1.Init.TimeTriggeredMode = DISABLE;
  hcan1.Init.AutoBusOff = DISABLE;
  hcan1.Init.AutoWakeUp = DISABLE;
  hcan1.Init.AutoRetransmission = ENABLE;
  hcan1.Init.ReceiveFifoLocked = DISABLE;
  hcan1.Init.TransmitFifoPriority = DISABLE;
  if (HAL_CAN_Init(&hcan1) != HAL_OK)
  {
    Error_Handler();
  }

  /* USER CODE BEGIN CAN1_Init 2 */
  CAN_FilterTypeDef  sFilterConfig;

  /*##-2- Configure the CAN Filter ###########################################*/
  sFilterConfig.FilterBank = 0;
  sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
  sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
  sFilterConfig.FilterIdHigh = 0x0000;
  sFilterConfig.FilterIdLow = 0x0000;
  sFilterConfig.FilterMaskIdHigh = 0x0000;
  sFilterConfig.FilterMaskIdLow = 0x0000;
  sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
  sFilterConfig.FilterActivation = ENABLE;
  sFilterConfig.SlaveStartFilterBank = 14;

  if(HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig) != HAL_OK)
  {
    /* Filter configuration Error */
    Error_Handler();
  }


  /*##-3- Start the CAN peripheral ###########################################*/
  if (HAL_CAN_Start(&hcan1) != HAL_OK)
  {
    /* Start Error */
    Error_Handler();
  }

  /* USER CODE END CAN1_Init 2 */

}

/**
  * @brief GPIO Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_GPIO_Init(void)
{

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOH_CLK_ENABLE();
  __HAL_RCC_GPIOA_CLK_ENABLE();

}

/* USER CODE BEGIN 4 */
HAL_StatusTypeDef CAN_Polling(void)
{

  /*##-4- Start the Transmission process #####################################*/
  TxHeader.StdId = 0x11;
  TxHeader.RTR = CAN_RTR_DATA;
  TxHeader.IDE = CAN_ID_STD;
  TxHeader.DLC = 7;
  TxHeader.TransmitGlobalTime = DISABLE;
  TxData[0] = 0x43;
  TxData[1] = 0x52;
  TxData[2] = 0x45;
  TxData[3] = 0x56;
  TxData[4] = 0x41;
  TxData[5] = 0x56;
  TxData[6] = 0x49;

  /* Request transmission */
  if(HAL_CAN_AddTxMessage(&hcan1, &TxHeader, TxData, &TxMailbox) != HAL_OK)
  {
    /* Transmission request Error */
    Error_Handler();
  }

  /* Wait transmission complete */
  while(HAL_CAN_GetTxMailboxesFreeLevel(&hcan1) != 3) {}

  /*##-5- Start the Reception process ########################################*/
  if(HAL_CAN_GetRxFifoFillLevel(&hcan1, CAN_RX_FIFO0) != 1)
  {
    /* Reception Missing */
    Error_Handler();
  }

  if(HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK)
  {
    /* Reception Error */
    Error_Handler();
  }

 /* if((RxHeader.StdId != 0x11)                     ||
     (RxHeader.RTR != CAN_RTR_DATA)               ||
     (RxHeader.IDE != CAN_ID_STD)                 ||
     (RxHeader.DLC != 7)                          ||
     ((RxData[0]<<8 | RxData[1]) != 0xCAFE))
  {
     Rx message Error
    return HAL_ERROR;
  }*/

  return HAL_OK; /* Test Passed */
}

/* USER CODE END 4 */

/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}

#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @PAram  file: pointer to the source file name
  * @PAram  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

The pins are no pull up no pull down

Hello,

I've already looked at your code from your attached main and you are using LoopBack mode.

So please review my answer in my previous comment:

  1. - You need to set new values for BS1, BS2 and CAN prescaler: see this thread: https://community.st.com/t5/stm32-mcus-products/can1-loopback-does-not-work-on-stm32f427/m-p/695622
  2. - You need to set the internal pull-up for CAN_Rx pin.

The code you shared don't give a full picture of all your configuration. You need to share your project including the ioc file.

EDIT: updated the correct link to the thread.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.