cancel
Showing results for 
Search instead for 
Did you mean: 

ARM Cortex M7

DCtech
Associate II

I was using stm32f4 on my project but now I want to use the h7 products. I am reading referance manual and watching some videos about the arm cortex m7, but I didnt understand completely about the CPU things. How can I learn the most basic way to understand its memory organization ?

This is one of the things i don't understand:

I also exemine the example of the stm32Cube with h7, every examples start with CPU_CACHE_Enable(); , Should I use the this line in every project and why I didnt understand this function using although reading referance manual ?

This discussion is locked. Please start a new topic to ask your question.
16 REPLIES 16

Hi Peter,

On https://www.st.com/en/microcontrollers-microprocessors/stm32h743ag.html#documentation I see Application Notes (5 of 52) and under the 5 appnotes I see Load More. When I click on Load More once, I see all 52 appnotes and no Load More. Within those 52 appnotes, there is no AN4891 (below is the list).

Jan

@Peter BENSCH​ 

AN3126 Audio and waveform generation using the DAC in STM32 products

   4.0   08 Jul 2020

AN5020 Digital camera interface (DCMI) on STM32 MCUs

   1.0   04 Aug 2017

AN1709 EMC design guide for STM8, STM32 and Legacy MCUs

   3.1   09 May 2019

AN1181 Electrostatic discharge sensitivity measurement

   1.6   11 Jul 2017

AN5543 Enhanced methods to handle SPI communication on STM32 devices

   2.0   05 Jul 2021

AN5342 Error correction code (ECC) management for internal memories protection on STM32H7 Series

   2.0   09 Jan 2020

AN4566 Extending the DAC performance of STM32 microcontrollers

   3.0   19 Sep 2019

AN5348 FDCAN peripheral on STM32 devices

   1.0   07 Oct 2019

AN5405 FDCAN protocol used in the STM32 bootloader

   2.0   28 Jun 2021

AN4776 General-purpose timer cookbook for STM32 microcontrollers

   3.0   16 Jul 2019

AN5200 Getting started with STM32H7 Series SDMMC host controller

   1.0   30 Nov 2018

AN4938 Getting started with STM32H74xI/G and STM32H75xI/G hardware development

   5.0   21 Jan 2020

AN4990 Getting started with sigma-delta digital interface on applicable STM32 microcontrollers

   1.0   05 Apr 2018

AN5354 Getting started with the STM32H7 Series MCU 16-bit ADC

   1.0   23 Mar 2020

AN4539 HRTIM cookbook

   4.0   23 Apr 2021

AN4750 Handling of soft errors in STM32 applications

   2.1   11 Jul 2017

AN4996 Hardware JPEG codec peripheral in STM32F76/77xxx and STM32H743/53/45/55/47/57/50/A3/B3/B0xx microcontrollers

   3.0   24 Dec 2019

AN4803 High-speed SI simulations using IBIS and board-level simulations using HyperLynx® SI on STM32 MCUs and MPUs

   2.0   06 Sep 2019

AN2834 How to get the best ADC accuracy in STM32 microcontrollers

   7.0   01 Jun 2021

AN4229 How to implement a vocoder solution using STM32 microcontrollers

   1.2   20 Apr 2020

AN4221 I2C protocol used in the STM32 bootloader

   10.0   11 Jun 2021

AN5027 Interfacing PDM digital microphones using STM32 MCUs and MPUs

   2.0   17 Jul 2019

AN5156 Introduction to STM32 microcontrollers security

   6.0   06 Jul 2021

AN4861 LCD-TFT display controller (LTDC) on STM32 MCUs

   3.0   15 Jul 2020

AN4839 Level 1 cache on STM32F7 Series and STM32H7 Series

   2.0   07 Mar 2018

AN4838 Managing memory protection unit in STM32 MCUs

   5.0   20 Sep 2021

AN5312 Migration from RevY to RevV for STM32H743/753 and STM32H750 Value line microcontrollers

   1.0   05 Apr 2019

AN5293 Migration guide from STM32F7 Series and STM32H743/753 line, to STM32H7A3/7B3 and STM32H7B0 Value line devices

   5.0   12 Oct 2020

AN4936 Migration of microcontroller applications from STM32F7 Series to STM32H743/753 line

   2.0   15 Sep 2020

AN4635 Minimization of power consumption using LPUART for STM32 microcontrollers

   5.0   28 Nov 2019

AN2867 Oscillator design guide for STM8AF/AL/S, STM32 MCUs and MPUs

   15.0   07 Oct 2021

AN4760 Quad-SPI interface on STM32 microcontrollers and microprocessors

   4.0   13 Dec 2021

AN5073 Receiving S/PDIF audio stream with the STM32F4/F7/H7 Series

   2.0   28 Jun 2018

AN4286 SPI protocol used in the STM32 bootloader

   10.0   11 Jun 2021

AN5224 STM32 DMAMUX: the DMA request router

   4.0   09 Jun 2020

AN4908 STM32 USART automatic baud rate detection

   2.0   15 Oct 2020

AN4013 STM32 cross-series timer overview

   9.0   01 Jun 2021

AN4899 STM32 microcontroller GPIO configuration for hardware settings and low-power consumption

   2.0   12 Aug 2021

AN4989 STM32 microcontroller debug toolbox

   3.0   28 Jan 2021

AN4230 STM32 microcontroller random number generation validation using the NIST statistical test suite

   6.0   18 Aug 2020

AN2606 STM32 microcontroller system memory boot mode

   51.0   26 Oct 2021

AN5033 STM32Cube MCU Package examples for STM32H7 Series

   7.0   30 Jun 2020

AN5337 STM32H7 Series lifetime estimates

   2.0   21 Jul 2020

AN2639 Soldering recommendations and package information for Lead-free ECOPACK MCUs and MPUs

   7.0   11 Oct 2019

AN5036 Thermal management guidelines for STM32 applications

   3.0   23 Apr 2019

AN3155 USART protocol used in the STM32 bootloader

   14.1   11 Jun 2021

AN3156 USB DFU protocol used in the STM32 bootloader

   12.1   08 Jun 2021

AN5225 USB Type-C Power Delivery using STM32 MCUs and MPUs

   5.0   13 Oct 2021

AN4879 USB hardware and PCB guidelines using STM32 MCUs

   4.0   19 Dec 2018

AN4759 Using the hardware real-time clock (RTC) and the tamper management unit (TAMP) with STM32 microcontrollers

   7.0   21 Sep 2021

AN5690 VREFBUF peripheral applications and trimming technique

   2.0   09 Dec 2021

AN4655 Virtually increasing the number of serial communication peripherals in STM32 applications

   1.1   11 Jul 2017

TDK
Guru

It's under "Application Notes for related Tools & Software (30 of 30)".

However, depending on what buttons you click and how the website feels at the current moment, it may or may not be available with a "Load more" button.

0693W00000HqmfOQAR.png 

0693W00000HqmfsQAB.png

If you feel a post has answered your question, please click "Accept as Solution".

Thanks, Jan,

Now it gets really mysterious, because I had definitely seen the AN4891 with my own eyes in this list yesterday - most strange.

Funnily enough, it shows up in the tab Tools & Software, under

MCU & MPU Embedded Software > X-CUBE-PERF-H7.

In X-CUBE-PERF-H7 it is then finally also to be found. Perhaps a little unfortunate positioned.

Regards

/Peter

@Community member​ 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

> It's under "Application Notes for related Tools & Software (30 of 30)".

Indeed. What an inappropriate place.

> depending on what buttons you click

The whole design of those product folders is a fail. "Modern and trendy", but not functional. ST won't listen to us anyway, I gave up.

JW

Peter,

> Perhaps a little unfortunate positioned.

That's not "little". It completely defeats the point of the AN. If it's hidden at an unexpected place, it's as good as it never existed.

Jan

@Peter BENSCH​ 

I hate the site design as well. It takes 2-3 seconds to load, tabs disappear while you are viewing it, things actively move in unexpected ways at certain points while you scroll down the page, the header remains onscreen and takes up viewing space when you don't want it to be there.
The only way such a design would be deemed adequate is if the person making the decision never actually needs to use the site. Unfortunately, I suspect most software decisions in large companies are made by such a person.
The saving grace of ST is that its hardware is really quite good and, up until a couple years ago, relatively cheap and readily available.
If you feel a post has answered your question, please click "Accept as Solution".

Jan,

I agree with you guys completely.

However, with this discussion we have left the original question or the topic of the TO again, haven't we?

/Peter

@Community member​ 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.