2021-10-05 5:10 AM
Hi All,
I would like to configure my ADC such that it is able to read from 2 channels. And that the conversion of the channels will be stored in the memory through DMA. But most importantly, I want the conversion to be triggered by a TIMer's rising/falling edge.
So basically multichannel ADC conversion triggered by timer and stored through DMA.
Can anyone point me in the right direction to look at, links, books? etc. I am presently working with an STM32F031C6 MCU.
Many thanks
2021-10-05 5:59 AM
Hi @BoboyeOkeya ,
A step by step hands-on is described in this video: Trigger Periodic ADC Conversions.
As it is based on STM32CubeMX/STM32CubeIDE, you can select your target MCU but the steps will be almost the same.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-10-05 6:36 AM
Hi Amel,
This has been very useful.
Can you also help with links to a multchannel ADC using DMA and timer trigger?
Many thanks.
2021-10-05 7:50 AM
The video ADC DMA TIM HAL lab will answer your need.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-10-11 7:26 AM
Hello @BoboyeOkeya ,
Additionally to previous post, you can refer to examples in FW packages.
For example in STM32F0 FW package:
Using ADC LL driver:
...\Firmware\Projects\STM32F072RB-Nucleo\Examples_LL\ADC\ADC_SingleConversion_TriggerTimer_DMA
Using ADC HAL driver:
a combination of these 2 examples using DMA and trigger from timer:
...\Firmware\Projects\STM32F072B-Discovery\Examples\ADC\ADC_DMA_Transfer
...\Firmware\Projects\STM32F072B-Discovery\Examples\ADC\ADC_TriggerMode
About conversion triggered by timer rising/falling edge:
It is possible using these literals:
LL driver: LL_ADC_REG_TRIG_EXT_RISINGFALLING
HAL driver: AdcHandle.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISINGFALLING;
Best regards
Philippe