2023-04-13 6:39 AM
Adc start conversion on Tim1_CC4 (Input capture compare) doesn't work.
I'm using STM32G051k8, Input capture compare works fine on Tim 1 Ch4 (I @read a correct input value) but doesn't generate an Adc start events.
Can you help me?
Thank you in advanced.
Best regards
2023-04-14 6:30 AM
Hello @Community member ,
Maybe this wiki article on ADC topic can help you
Regards
Michael
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-17 6:01 AM
Hello Hello Michael I read the wiki article but the problem persist.
The Ch4 of Timer 1 when is configured in input capture compare mode doesn't trigger a Adc start. If I configure the external trigger of adc as TIM1_TRGO2 (Reset,gated etc.) there aren't any problems Adc start the conversion.
If I move the setting of external trigger to TIM1_CC4 the adc doesn't trigger a conversion even if the Tim1 Input capture compare is working regular because the irq of capture compare in tim1 is active and i can read correctly a value on the TIM1_CCR4 register.
Do you have any suggestion?
Regards
Stefano
2023-05-17 7:26 AM
This is most probably case of incorrect documentation and the ADC is *not* triggered by TIMx_CCx event, but the TIMx_OCx signal, i.e. the signal which goes to the output pins from the Output stage of given TIMx channel.
This has several ramifications:
ST perpetuates this error (in some STM32 families using "TIMx_CHx" instead of "TIMx_CCx", not making it any better) ever since the first STM32F1. There are numerous threads in this forum, through the years, involving ST insiders.
JW
@Imen DAHMEN
@Vincent Onde
2023-05-17 7:47 AM
Thank you very much @Community member
you were very clear.
Regards
Stefano