2022-07-30 04:09 AM
Using the STM's CubeMx HAL, I generate audio using PWM from a raw wav file at 8bit 44100hz but I am clearly using the DMA the wrong way. The resulting audio is fine but the solution has an unnecessary overhead.
I am using a circular DMA with one 8bit value in it's buffer array, and repeat this pulse until Timer5 clock is reset. The resulting audio is fine but the Timer interrupt is fired and processed too often at 44.1khz, hogging precious cycles.
audio_t audio_ch1;
#define SOMESIZE somesize
uint8_t audio_buf[SOMESIZE]={.........};
uint32_t audio_bufsize = SOMESIZE;
int main(void)
{
HAL_Init();
SystemClock_Config();
PeriphCommonClock_Config();
MX_GPIO_Init();
MX_TIM1_Init();
MX_TIM5_Init();
HAL_TIM_RegisterCallback(&htim5, HAL_TIM_PERIOD_ELAPSED_CB_ID,
&TIM5_PeriodElapsedCallback);
/* currently redundant
HAL_TIM_RegisterCallback(&htim1, HAL_TIM_PWM_PULSE_FINISHED_CB_ID,
&PWM_PulseFinishedCallback); */
HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, (uint32_t*) &audio_ch1.ptr, 1);
HAL_TIM_Base_Start_IT(&htim5);
HAL_TIM_Base_Start_IT(&htim1);
playSound(audio_buf, audio_bufsize, PLAY_ONCE, 1);
return 0;
while (1) {
}
}
/*
currently redundant
void PWM_PulseFinishedCallback(TIM_HandleTypeDef *htim) {
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1)
audio_ch1.pulseFinished = true;
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_3)
audio_ch2.pulseFinished = true;
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_2)
{
audio_ch1.pulseFinished = true;
}
}
*/
int8_t emptyArray[10];
void TIM5_PeriodElapsedCallback(TIM_HandleTypeDef *htim) {
if ( audio_ch1.mode != NOT_PLAYING) {
if (audio_ch1.cnt >= audio_ch1.length) {
switch (audio_ch1.mode) {
case PLAY_LOOP:
audio_ch1.cnt = 0;
(*audio_ch1.state) = false;
break;
case PLAY_ONCE:
audio_ch1.cnt = 0;
audio_ch1.buffer = emptyArray;
audio_ch1.length = 10;
audio_ch1.mode = NOT_PLAYING;
(*audio_ch1.state) = false;
break;
default:
audio_ch1.cnt = 0;
break;
}
if (audio_ch1.length && audio_ch1.mode != NOT_PLAYING) {
audio_ch1.ptr = audio_ch1.buffer[audio_ch1.cnt++] ;
}
}
}
void playSound(const uint8_t *wav, uint32_t len, SfxMode mode, audio_t *audio) {
audio->cnt = 0;
audio->length = len;
audio->buffer = (uint8_t*) wav;
audio->mode = mode;
audio->state = state;
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/*AXI clock gating */
RCC->CKGAENR = 0xFFFFFFFF;
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Configure LSE Drive Capability
*/
HAL_PWR_EnableBkUpAccess();
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);
/** Macro to configure the PLL clock source
*/
__HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSE);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_LSI
|RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.LSIState = RCC_LSI_ON;
RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 12;
RCC_OscInitStruct.PLL.PLLN = 280;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_1;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7) != HAL_OK)
{
Error_Handler();
}
HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_HSE, RCC_MCODIV_1);
}
void PeriphCommonClock_Config(void)
{
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/** Initializes the peripherals clock
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_OSPI|RCC_PERIPHCLK_ADC
|RCC_PERIPHCLK_SDMMC;
PeriphClkInitStruct.PLL2.PLL2M = 12;
PeriphClkInitStruct.PLL2.PLL2N = 280;
PeriphClkInitStruct.PLL2.PLL2P = 4;
PeriphClkInitStruct.PLL2.PLL2Q = 4;
PeriphClkInitStruct.PLL2.PLL2R = 14;
PeriphClkInitStruct.PLL2.PLL2RGE = RCC_PLL2VCIRANGE_1;
PeriphClkInitStruct.PLL2.PLL2VCOSEL = RCC_PLL2VCOWIDE;
PeriphClkInitStruct.PLL2.PLL2FRACN = 0;
PeriphClkInitStruct.OspiClockSelection = RCC_OSPICLKSOURCE_PLL2;
PeriphClkInitStruct.SdmmcClockSelection = RCC_SDMMCCLKSOURCE_PLL2;
PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_PLL2;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
}
void MX_TIM1_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0}
htim1.Instance = TIM1;
htim1.Init.Prescaler = PWM_PRESCALER;
htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
htim1.Init.Period = PWM_PERIOD;
htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim1.Init.RepetitionCounter = 0;
htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_Init(&htim1) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_OC1;
sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_ASSYMETRIC_PWM1;
sConfigOC.Pulse = 0;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_ENABLE;
sConfigOC.OCIdleState = TIM_OCIDLESTATE_SET;
sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
{
Error_Handler();
}
sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
sBreakDeadTimeConfig.DeadTime = 0;
sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_LOW;
sBreakDeadTimeConfig.BreakFilter = 0;
sBreakDeadTimeConfig.Break2State = TIM_BREAK2_DISABLE;
sBreakDeadTimeConfig.Break2Polarity = TIM_BREAK2POLARITY_LOW;
sBreakDeadTimeConfig.Break2Filter = 0;
sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_ENABLE;
if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
{
Error_Handler();
}
HAL_TIM_MspPostInit(&htim1);
}
static void MX_TIM5_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
htim5.Instance = TIM5;
htim5.Init.Prescaler = OC_PRESCALER;
htim5.Init.CounterMode = TIM_COUNTERMODE_UP;
htim5.Init.Period = OC_PERIOD;
htim5.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim5.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_Base_Init(&htim5) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim5, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_OC1;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim5, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
}
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOI_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOG_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOE_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOK_CLK_ENABLE();
__HAL_RCC_GPIOJ_CLK_ENABLE();
/*Configure GPIO pin : PA8 */
GPIO_InitStruct.Pin = GPIO_PIN_8;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF0_MCO;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
2022-08-01 07:13 AM
I don't use Cube.
If you've set DMA to transfer N words (or halfwords, whatever is set), and it's triggered by Update event of TIM1 which has TIM1_RCR=M, then the DMA Transfer Complete interrupt is invoked after (M+1)*N periods of TIM1.
Note, that TIMx_RCR is unconditionally preloaded.
JW
2022-08-01 04:57 PM
Thanks for all your helpwaclawek.jan
I'm pretty happy with the results I've got. However any more than 2 repetitions and the output gets noisy but I feel that the audio and the cycles needed to increment the buffer are good enough for what I require... I now have another issue which I'm going to post but don't worry I'm not gonna quote any cubemx hal code 🙂