cancel
Showing results for 
Search instead for 
Did you mean: 

will ST release a version of MC SDK for LinuX?

MMa.1893
Associate III

Hi, I'm a fans of STM32, i can write my code under linux well. But know, i wanna use adv motor control, i know ST has a MC SDK, but it for windows only?

i hope i can design my motor program on Linux.

Thank you !

1 ACCEPTED SOLUTION

Accepted Solutions
Laurent Ca...
Lead II

Dear MMa.1893

Next release has been a little bit postponed and this feature will be probably integrated only in the next version.

Therefor, a full tools suite linux integration is not planned on the short term.

Best Regards

Laurent Ca...

View solution in original post

11 REPLIES 11
cedric H
ST Employee

Hello

yes we will :)

Unfortunately, it will not be ready soon :( - The target is Q2 2020 -

We are developing a new MotorControl Workbench from scratch that will be available for all platforms by construction. (Linux, MacOs, Windows).

In the meantime, a new MotorControl Monitor is also under construction and will be available for Linux too. It will be publicly available Q1 2020.

Regards

Cedric

wow!!

I am very excited. Hope the new tools will be more friends to linux command line tools chains..

any beta or preview version now? ��

any update now?

We are working on it. now.. it should be for Q3 2020.

any update now? ^_^

Hello,

We are working on the new MC Workbench generation as planned. Unfortunately the very first version we are preparing now has some limitation and will work only with windows :(. But for sure we will solve this issue before the official release.

A question for you as well, which STM32 family are you using?

Thanks and best regards,

Claire

for now, STM32F3(stm32f303re) for adv bldc control

any update now?