2024-07-29 12:08 PM - edited 2024-07-29 12:09 PM
Good afternoon. I am starting to write a final qualifying paper using BG431-ESС1 and a BLDC motor. I profiled the engine in motor profiler 5.4.8, generated the code in mcsd 5.4.8 and checked it in it, the engine started. After that, I generated the code in mcsd 6.3 with a six-step control algorithm. Now I want to run this code using KeilV5 with HAL. But I don't understand what I need to add to main.c to make this happen. Perhaps my request is too...., because I just started studying stm32 and avr in general. I hope for any help, thank you!