cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-F446ZE for dual motor configuration in STM32 MC Workbench

apexyz
Associate II

Does anybody know if control board NUCLEO-F446ZE and power board X-NUCLEO-IHM07M1 can be configured to support 2 motors (FOC) in STM32 MC Workbench? 

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @apexyz,

You can filter control boards that support dual drive by using "Filters" feature (NUCLEO-F446ZE board is not available on current MC Workbench version):

GMA_0-1736259924470.png

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

View solution in original post

3 REPLIES 3
samcaras
Associate

@apexyzdgme wrote:

Does anybody know if control board NUCLEO-F446ZE and power board X-NUCLEO-IHM07M1 can be configured to support 2 motors (FOC) in STM32 MC Workbench? 


Yes, the NUCLEO-F446ZE and X-NUCLEO-IHM07M1 can be configured to support two motors (FOC) in STM32 MC Workbench. You would need to set up two motor configurations in the MC Workbench and ensure proper wiring and power handling for both motors.

Thanks for the prompt reply! But when I config 2 motors in MC Workbench, I got the following error message:

apexyz_0-1736129629505.png

How to set up the wiring and power handling properly?

Hello @apexyz,

You can filter control boards that support dual drive by using "Filters" feature (NUCLEO-F446ZE board is not available on current MC Workbench version):

GMA_0-1736259924470.png

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA