cancel
Showing results for 
Search instead for 
Did you mean: 

Motor profiler restrictions

GJamo.1
Associate II

I'm using motor profiler for the motor control. I have the following hardware components:

  • STM32 Nucleo-F4446RE
  • X-NUCLEO-IHM16M1
  • Mitoot motor

In the motor profiler, it mentions that IHM16M1 can only work sith STM32 Nucleo-G4 and that F4 and IHM16 combined is not supported.

Is there a workaround available to test the motor despite this limitation?"

1 ACCEPTED SOLUTION

Accepted Solutions
cedric H
ST Employee

Hello @GJamo.1​,

Which version of the MCSDK do you use?

I just checked with the MCSDK 6.1.2, and the combinaison Nucleo-F4446RE+X-NUCLEO-IHM16M1 is proposed by the profiler.

Regards

Cedric

View solution in original post

2 REPLIES 2
cedric H
ST Employee

Hello @GJamo.1​,

Which version of the MCSDK do you use?

I just checked with the MCSDK 6.1.2, and the combinaison Nucleo-F4446RE+X-NUCLEO-IHM16M1 is proposed by the profiler.

Regards

Cedric

GJamo.1
Associate II

Thanks for the info