In the MC workbench, I get compilation error when enabling open loop mode in FOC for a PMSM with encoder. the OpenLoop_handle OpenLoop_ParamsM1 constants are not defined
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-06-08 8:27 AM
T
OpenLoop_Handle_t OpenLoop_ParamsM1 =
{
.hDefaultVoltage = OPEN_LOOP_VOLTAGE_d,
.VFMode = OPEN_LOOP_VF,
.hVFOffset = OPEN_LOOP_OFF,
.hVFSlope = OPEN_LOOP_K
};
Constant are undeclared. Any ideas what should be those value? I also don't understand how to set the offset angle between encoder Z channel and motor phase reference
In addition I can't find where to define the open voltage or current in Motor Pilot GUIs.
Many thanks
David
- Labels:
-
STM32 Motor Control
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-06-09 8:05 AM
Ok, I found the code documentation and figured a few things :grinning_face_with_sweat:
What is the measurement unit of OPEN_LOOP_VOLTAGE_d ?
Still the question about the encoder remains. I understand the encoder control force an alignement each time. Is the Z channel of any use in software?