2024-01-29 3:35 AM
hello st community,
I am experiencing issues while trying to operate the BR2804 1700Kv BLDC motor with the IHM07M1 motor controller and nucleo G071RB board. we are just using the software like cube mx , cube ide to genarate code . while using g071rb with IHM07M1 the motor only rotates for a short duration (2 or 3 seconds) before encountering startup failure or speed feedback issues.
what will be the issue , can anyone help me with this ,
2024-01-29 9:39 PM
motor is working now with some changes , but it's max rpm is 8500 . after that it shows over current. and also unable to change the speed in faster way , what will be its reason ?