2021-08-06 9:54 PM
I have a design which uses STM32G431C6T6 (LQFP48). In the MCSDK, it is possible to select only between STM32G431RB (LQFP64) or STM32G431CB (UFQFPN48).
Is it somehow possible to configure/hack the MCSDK use some different MCU? This LQFP48 version of the STM32G431 is very close to the UFQFPN model anyway..
Solved! Go to Solution.
2021-08-09 4:05 AM
Dear @jouko.perkkio
The STM32G431C6T6 has 32 KB of Flash memory while the STM32G431CB has 128. This is not a problem for the STM32 MC-SDK.
The STM32G431C6T6 also has an additional HW accelerator (CORDIC).
But the packages are the same.
Therefore, if you select STM32G431CB, the STM32 MC-SDK should work fine.
Come back here if it doesn't.
Do not hesitate to check "best answer" if this answer is OK for you.
Best regards
2021-08-09 4:05 AM
Dear @jouko.perkkio
The STM32G431C6T6 has 32 KB of Flash memory while the STM32G431CB has 128. This is not a problem for the STM32 MC-SDK.
The STM32G431C6T6 also has an additional HW accelerator (CORDIC).
But the packages are the same.
Therefore, if you select STM32G431CB, the STM32 MC-SDK should work fine.
Come back here if it doesn't.
Do not hesitate to check "best answer" if this answer is OK for you.
Best regards