2021-09-28 1:44 AM
My compensation today:
if(I->a >= deadband_thresholde)
{
compare_u += dead_time_comp;
}
else if(I->a <= -deadband_thresholde)
{
compare_u -= dead_time_comp;
}
if(I->b >= deadband_thresholde)
{
compare_v += dead_time_comp;
}
else if(I->b <= -deadband_thresholde)
{
compare_v -= dead_time_comp;
}
if(I->c >= deadband_thresholde)
{
compare_w += dead_time_comp;
}
else if(I->c <= -deadband_thresholde)
{
compare_w -= dead_time_comp;
}
__HAL_TIM_SET_COMPARE(htim, TIM_CHANNEL_U, compare_u);
__HAL_TIM_SET_COMPARE(htim, TIM_CHANNEL_V, compare_v);
__HAL_TIM_SET_COMPARE(htim, TIM_CHANNEL_W, compare_w);
2021-09-28 2:07 AM
Try to draw a timing diagram to show us what is the problem and what do you want to achieve.
JW
2021-09-28 3:33 AM
Hello,
If your question is about hardware capabilities of the STM32G4 to support dead time compensation algorithm, the answer is yes, it can be done with STM32G4.
In our current MC-SDK, we did not implement it.
Now, your question seems to be more related to the Timer specification itself, and I am not sure it is the right forum to ask.
Regards
Cedric
2021-09-28 3:55 AM
The question is timer specific, but I also wonder how people do dead time compensation in their projects. I have setup the dead time in hardware and want the regulator to compensate for this deadtime.
-Lars
2021-09-28 4:06 AM
2021-09-28 4:27 AM
Lars,
What you've drawn appears to match the Asymmetric PWM mode, read TIM chapter's subchapter of this name in the RM. However, only 2 asymmetric outputs are available per timer, as this mode combines 2 channels into 1.
Note, that deadtime insertion as described in the Complementary outputs and dead-time insertion subchapter shifts only one edge of the signal appearing on the output pin.
JW
2021-09-28 5:41 AM
Hello,
If three phases are needed with this asymmetric shape, it is possible to achieve that with the help of a DMA that will reconfigure the CCR[1-3] registers.
The idea is that when the timer reach the auto reload value, a DMA event is generated and will copy 3 news values to the CCR[1-3]. Same has to be done when the counter reach 0.
Cedric.
2021-09-28 6:30 AM
Thanks Cedrick,
That's a good idea. I will try to do that.
Lars