2023-11-06 08:16 AM
Hi,
I was trying to use Profiler in Motor Pilot to find motor settings for the evaluation board (ESPIN32F0602S1). However, I found out that the current version of Pilot (V1.2.4 from MC Workbench V6.2) didn’t support the evaluation board (ESPIN32F0602S1). MC Workbench showed the error message, "Motor Profiler is available only in 3 shunt current sensing. Motor profiler is not available for the mcu.". ESPIN32F0602S1 only has one shunt current sensing.
Is there a way to use Profiler with ESPIN32F0602S1?
Thanks,
2023-11-06 08:36 AM
Hello @TomChu ,
to be compatible with the profiler, the board must be 3Shunt and have an FPU. This board does not do 3Shunt and its MCU (STM32F0) does not have an FPU.
Regards