cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link V2 Not Connecting to STM32F303RCT7

udhayakumar
Associate II

HI,

I am facing an issue where my ST-Link V2 is not detected in STM32CubeIDE while trying to connect to my STM32F303RCT7 board. 

Below are the details:

:small_blue_diamond:**Issue Description:

** - ST-Link V2 is connected via USB, but it is not detected in STM32CubeIDE.

- ST-Link Utility/STM32CubeProgrammer also does not recognize the device.

- I have checked all connections (SWDIO, SWCLK, VCC, GND).

- The board is powered correctly (3.3V).

:small_blue_diamond:**Troubleshooting Steps Taken:

** :white_heavy_check_mark: Reinstalled ST-Link drivers

:white_heavy_check_mark:Tried different USB cables and ports

:white_heavy_check_mark:Updated ST-Link firmware

:white_heavy_check_mark:Checked connections with a multimeter

:small_blue_diamond:**System Details:**

- **MCU:** STM32F303RCT7 -

**Debugger:** ST-Link V2 -

**OS:** Windows-

**STM32CubeIDE

 Please guide me on how to resolve this issue.

                                                                       Thank you for your support.

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

with a Clone version, the connection may not work. So please make sure to use a genuine version.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
Andrew Neil
Super User

Welcome to the forum.

Please see: How to write your question to maximize your chances to find a solution

 


@udhayakumar wrote:

my ST-Link V2 is not detected in STM32CubeIDE .


What, exactly, do you mean by that?

Show the error message(s) you get.

What CudeIDE version?

Is it a genuine ST-Link?

https://community.st.com/t5/stm32-mcus/how-to-recognize-a-genuine-st-link-v2-versus-a-cloned-one/ta-p/49471

Is the ST-Link detected by the PC?

https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/tac-p/698105/highlight/true#M956

 


@udhayakumar wrote:

my STM32F303RCT7 board. 


What board? Please give details

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
STTwo-32
ST Employee

Hello @udhayakumar and welcome to the ST Community.

Could you please share a picture of your ST-LINK V2. I think you are using a Clone version. More details available on the article How to recognize a genuine ST-LINK/V2 versus a clo... - STMicroelectronics Community.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

HI bro,

yes,i used clone version.

Best Regards

udhayakumar

Hi bro,

i used clone version.

 

with a Clone version, the connection may not work. So please make sure to use a genuine version.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

AScha.3
Super User

Hi,

>does not recognize the device

What ? st-link or target cpu ?

Try : CubeProgrammer, connect : normal + software reset . Then show, what its telling...

If you feel a post has answered your question, please click "Accept as Solution".