cancel
Showing results for 
Search instead for 
Did you mean: 

Firmware error detected by Profiler n ST Motor Pilot V1.2.4

TomChu
Associate

Hi, 

I was trying to use Profiler in Motor Pilot to find motor settings for the evaluation board (ESPIN32F0602S1). However, I found out that the current version of Pilot (V1.2.4 from MC Workbench V6.2) didn’t support the evaluation board (ESPIN32F0602S1). MC Workbench showed the error message, "Motor Profiler is available only in 3 shunt current sensing. Motor profiler is not available for the mcu.". ESPIN32F0602S1 only has one shunt current sensing.

Is there a way to use Profiler with ESPIN32F0602S1?

Thanks,

1 REPLY 1
Zied b.
ST Employee

Hello @TomChu ,
to be compatible with the profiler, the board must be 3Shunt and have an FPU. This board does not do 3Shunt and its MCU (STM32F0) does not have an FPU.
Regards

If you agree with my answer, please accept it by clicking on "Accept as solution".