cancel
Showing results for 
Search instead for 
Did you mean: 

Errors in stmcubeide when generating motor profiler code with MC Workbench 6.3.0

hashiR
Associate III

hello community,

issue : Error in stmcubeide when generating motor profiler code with MC Workbench 6.3.0 

what will be the reason ?

 

 

 

hashiR_0-1726039623773.png

4 REPLIES 4
GMA
ST Employee

Hello @hashiR and welcome to ST community,

Could please add more detail about your use case as described in this post?

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA
Andrew Neil
Evangelist III

@hashiR wrote:

what will be the reason ?


Exactly as it says: you have not defined those symbols - therefore, they are undefined.

Have you omitted the file(s) which would define them?

 

hashiR
Associate III

When I check the 'Motor Profiler' box in Motor Control Workbench (v6.3.0) and generate the code, errors appear in STM32CubeIDE (v1.16.0). However, when the 'Motor Profiler' box is unchecked, everything works fine.

hashiR_0-1726638012551.png

 

GMA
ST Employee

Hello @hashiR,

What is the used ST platform?

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA