2024-09-11 12:31 AM - last edited on 2024-09-11 12:35 AM by Peter BENSCH
hello community,
issue : Error in stmcubeide when generating motor profiler code with MC Workbench 6.3.0
what will be the reason ?
2024-09-11 5:11 AM
2024-09-11 5:33 AM
@hashiR wrote:what will be the reason ?
Exactly as it says: you have not defined those symbols - therefore, they are undefined.
Have you omitted the file(s) which would define them?
2024-09-17 11:16 PM
When I check the 'Motor Profiler' box in Motor Control Workbench (v6.3.0) and generate the code, errors appear in STM32CubeIDE (v1.16.0). However, when the 'Motor Profiler' box is unchecked, everything works fine.
2024-09-17 11:22 PM
Hello @hashiR,
What is the used ST platform?