cancel
Showing results for 
Search instead for 
Did you mean: 

ioc file not generated from Motor Control Workbench - template inclusion failed

KStew.1
Associate III

Using Version: 6.3.2

I have a custom motor and a custom inverter board, importing these works fine in my project but when I try to generate the project I get the following:

2025-03-17 17:54:58,571 ERROR [LineInfo_to_exitCode.manage_IocGenerationError] Unable to generate ioc file due to: Template inclusion failed (for parameter value "STM32F769NI/STM32F769NI - 216 MHz - int.ftl"):...

I tried changing the MCU on my inverter to see if this was specific to a board and I keep getting the same bug. Please help :)

 

3 REPLIES 3
GMA
ST Employee

Hello @KStew.1,

Supported mcu are located on "MC_SDKToolDirectory\Utilities\PC_Software\STMCWB\assets\hardware\mcu" directory.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA
KStew.1
Associate III

The STM32F769NIHx JSON file is in that folder, this issue persists

Hello @KStew.1,

Can you share your custom board .json file and your associated .stwb6 file?

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA