STM32 MCUs Machine learning & AI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Edge AI for all. NanoEdge AI Studio autoML tool, now free for STM32 and open to all ARM Cortex-M bas

NanoEdge AI Studio v4.3 is now offered for free to all engineers, giving them the opportunity to create highly efficient TinyML libraries that can be deployed on Cortex-M based microcontrollers. In addition, other enhancements have been integrated to...

ST30449_nanoedge-ai-studio-motor (2).jpg ST30449_nanoedge-ai-studio-motor (2).jpg

https://wiki.st.com/stm32mcu/wiki/AI:How_to_perform_motion_sensing_on_STM32L4_IoTnode I'm using X-CUBE_AI 7.1.0 but having trouble compiling this example project for motion detection.

ai_input[0].n_batches = 1; 'ai_buffer' {aka 'struct ai_buffer_'} has no member named 'n_batches'network.hAI_DEPRECATED#define AI_NETWORK_IN \ ai_network_inputs_get(AI_HANDLE_NULL, NULL)This comes up invalid initializer error.Any ideas? The initial c...

RBenf.11 by Associate
  • 748 Views
  • 5 replies
  • 0 kudos

Resolved! NanoEdgeAIStudio�?�性能�?�関�?�る�?�?��?��?�?� Inquire about Performance of the NanoEdgeAIStudio.

詳�?��??調�?��?��?��?�際�?�, �?明�?�点�?��?��?��?��?��?��?��?��?�, �?��?�度�?�連絡致�?��?��?��?�。以下�?�3点�?��?��?��?��?�回答を�?�願�?�致�?��?��?�。​NanoedgeAIStudio�?�必�?メモリ�?��?��??ら�?�?時系列データ�?�対応�?��?��?�る�?�?​目安�?�良�?��?��?�?一�?�当�?�り�?�価格を�?��?��?��?��?�?​2月24日...

I can't program FP-AI-MONITOR binary.

I am trying AI-MONITOR1 using STWIN Starter Kit.I am referring to the URL below.AI:FP-AI-MONITOR1 �?��?��?�?� - STM32MCUSection 2.3.2 states that the application is flashed on the sensor board, but it cannot be programmed because the memory capacity ...

0693W00000Y9QhPQAV.png
TShun.1 by Associate
  • 183 Views
  • 1 replies
  • 0 kudos

STM32Cube.AI Developer Cloud API

Hello,Taking a look at the new STM32Cube.AI Developer Cloud service, here it is said that it has an API for integration, but the API documentation seems to have just login-related functionality.Is the full API available yet?, if not, when will it be?...

ASalc.1 by Associate III
  • 303 Views
  • 2 replies
  • 0 kudos