cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H747 DSI 2-Lane Mode Issues with CO5300 Display Driver

amattes
Associate II

Hello! I am encountering some issues when trying to run 2-Lane DSI with an STM32H747.

Current Hardware Configuration:

  • MCU: STM32H747 (using the Cortex-M7 core)
  • Display Driver: Chipone CO5300 OLED Display Driver
  • Display Panel: Round TOH143XRT-01CG2 1.43" 466×466 AMOLED
  • Interface: MIPI DSI (adapted command mode)

 

Issue I am experiencing:

I have successfully implemented 1-lane DSI communication between the STM32H747 and CO5300 display driver. However, when I configure both the STM32 DSI host and CO5300 for 2-lane operation, the display is not responsive (black screen / nothing being displayed)

 

The display pipeline works as follows:

  1. DMA2D → Performs 2D graphics operations and copies framebuffer data to SRAM
  2. LTDC → Reads framebuffer from memory, performs layer blending, generates parallel RGB pixel stream (HSYNC, VSYNC, DE, pixel clock, RGB data)
  3. DSI Wrapper → Converts LTDC parallel RGB stream into a format suitable for DSI host
  4. DSI Host → Packetizes pixel data into MIPI DSI packets, serializes data through D-PHY lanes
  5. CO5300 → Receives DSI packets, writes pixel data to internal GRAM, drives AMOLED panel

 

Configuration Details:

Clock Configuration:

  • HSE: 25 MHz external crystal
  • System Clock (SYSCLK): 400 MHz (via PLL1)
  • AHB/APB3 Clock: 200 MHz
  • DSI PLL:
  • Input: HSE / 25 = 1 MHz
  • PLLNDIV (N): 100
  • PLLIDF (IDF): 5 (÷5)
  • PLLODF (ODF): 0 (÷1)
  • DSI PHY Clock: 500 MHz (100 × 25 MHz / 5)
  • Lane Byte Clock: 62.5 MHz (500 MHz ÷ 8)
  • LTDC Pixel Clock (PLL3R): ~38.4 MHz
  • DSI TX Escape Clock Divider: 4 (for low-power mode commands, ~50 MHz / 4 = 12.5 MHz)

 

LTDC Configuration:

  • Mode: Primary Layer Format: RGB888 
  • Resolution: 466×466 pixels
  • Framebuffer: Located in D2 SRAM (0x30000000), MPU configured for write-through cacheable access
  • Timing Parameters:
  • HSYNC: 2 clocks
  • VSYNC: 2 lines
  • HBP (Horizontal Back Porch): 2 clocks
  • VBP (Vertical Back Porch): 2 lines
  • Active Width: 466 pixels
  • Active Height: 466 lines
  • Total Width: 470 clocks
  • Total Height: 470 lines

 

DSI Host Configuration:

  • Mode: Adapted Command Mode (DSI->MCR CMDM bit set, DSI->WCFGR DSIM bit set)
  • Virtual Channel: 0
  • Color Coding: RGB888 (24-bit)
  • Command Size (LCCR): 466 pixels
  • Number of Lanes (PCONFR_NL):
  • 1-Lane Mode: 0 (Works)
  • 2-Lane Mode: 1 (Fails)
  • PHY Timings (for 2-lane):
  • Clock Lane HS→LP Time: 35
  • Clock Lane LP→HS Time: 35
  • Data Lane HS→LP Time: 35
  • Data Lane LP→HS Time: 35
  • Stop Wait Time: 10
  • UIX4 (Unit Interval × 4): Calculated as (4000000 × IDF × (1 << ODF)) / ((HSE_VALUE / 1000) × PLLNDIV) = ~80
  • Clock Lane Mode: Continuous clock enabled (CLCR_DPCC bit set)
  • Low Power Commands: Enabled during initialization, disabled during refresh

 

DSI Initialization Sequence (2-Lane):

  1. Disable DSI
  2. Reset DSI wrapper
  3. Configure and enable DSI PLL (wait for PLLLS lock)
  4. Set TX Escape Clock divider to 4
  5. Configure number of lanes: DSI->PCONFR = 1 (2 lanes)
  6. Enable PHY digital section (PCTLR_DEN)
  7. Enable clock lane (PCTLR_CKE)
  8. Wait for stop state: Check DSI->PSR for PSS0 | PSS1 | PSSC (both data lanes + clock lane)
  9. Configure UIX4 timing
  10. Configure PHY HS↔LP transition timings (CLTCR, DLTCR)
  11. Configure clock lane continuous mode
  12. Configure adapted command mode parameters
  13. Enable DSI host and wrapper
  14. Start LTDC

 

CO5300 Configuration:

Lane Mode Register (LANESEL, 0x03):

Initialization Sequence:

  1. Hardware reset via GPIO (low 10ms, high 10ms)
  2. Unlock CMD2 page access (password: 0xF4=0x20, 0xF5=0xF0)
  3. Switch to OLED IP page (0xFE=0x21)
  4. Set lane mode: 0x03 = 0x01 (2-lane)
  5. Configure display timing, gamma, power settings
  6. Set memory access control (MADCTL 0x36 = 0x80)
  7. Set pixel format (COLMOD 0x3A = 0x55, RGB565)
  8. Set column address (CASET 0x2A): columns 6-471 (466 visible pixels with 6-pixel offset)
  9. Set page address (PASET 0x2B): rows 0-465
  10. Exit sleep mode (SLPOUT 0x11), wait 120ms
  11. Display ON (DISPON 0x29)

 

Observed Symptoms in 2-Lane Mode:

  1. Display remains black after initialization completes successfully OR Greenish screen appears (suggesting uninitialized framebuffer data is being transmitted)
  2. Initialization sequence does not timeout - all register checks pass (PLLLS lock, PSR stop states, etc.)

 

What I've Verified:

  • DSI PLL locks successfully (PLLLS bit set)
  • PHY stop state check passes for both lanes (PSS0, PSS1, PSSC all set)
  • DSI->PCONFR reads back 0x01 (2-lane mode confirmed)
  • CO5300 LANESEL register written with 0x01
  • Clock lane continuous mode enabled
  • PHY timings configured (HS↔LP transition times)
  • LTDC timing parameters unchanged between 1-lane and 2-lane modes
  • Same initialization sequence works perfectly in 1-lane mode

 

What I've Tried:

  • Configuring lane count before PHY enable
  • Configuring lane count after PHY enable
  • Both continuous and non-continuous clock modes
  • Verified UIX4 calculation matches STM32H747-Disco Example formula
  • Increased stop-state wait timeout
  • Verified all DSI error registers are clear (ISR0, ISR1)

 

Questions:

  1. Are there additional DSI wrapper or host registers that need adjustment for 2-lane mode? (Beyond PCONFR_NL)
  2. Does LTDC timing need adjustment when switching from 1-lane to 2-lane DSI? (Even though LTDC timing is independent of DSI lane count)
  3. Is there a specific initialization order required for 2-lane mode? (e.g., must lane count be set before or after PHY enable?)
  4. Are there any known errata for STM32H747 DSI 2-lane operation?
  5. Could this be a CO5300-specific issue with 2-lane initialization? (Though datasheet suggests it should work)

 

Any insights or suggestions would be greatly appreciated!

 

Thank you!   -AM

2 REPLIES 2
MM..1
Chief III

Hi i dont calculate all, but normal display work start with choice refresh rate. Your LTDC clock setup define it around 170Hz . Are you sure?

MOBEJ
ST Employee

Hello @amattes , 

Based on the STM32H747 DSI examples available for the STM32H747I-DISCO board, especially the OTM8009A display driver example, I recommend using it as a reference for both DSI and LTDC configuration. You can compare the example setup with your own panel datasheet and adapt the code accordingly.

In particular, please review the LCD_Init() function carefully, with special attention to:

  • LCD clock configuration
  • DSI mode configuration
  • DSI PHY HS2LP and LP2HS timings
  • LTDC timing and pixel clock setup
  • Lane configuration and command mode settings

GitHub links for DSI examples : STM32CubeH7/Projects/STM32H747I-DISCO/Examples/LCD_DSI at master · STMicroelectronics/STM32CubeH7

Br

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.