cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407 SPI Datasize and FSMC #WR operation DOUBLEs

jhl14
Associate II

Hi Team,

Basing on the lastest "STM32F4xx_StdPeriph_Driver" to Read SPI data and then write into external FSMC(8bit) device in the PWM interrupt like following .

//----------------------------------------------------------------------------------------------------

void TIM2_IRQHandler(void)

{

SPI1->DR = 0; // SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b;

FTadd = Word_Upload++; // #define FTadd (*( uint16_t *)0x64000002)

TIM_ClearITPendingBit(TIM2,TIM_IT_Update);

}

//----------------------------------------------------------------------------------------------------

But from the LA waveform below, both SPI clock and FSMC #WR ops doubled.0693W000006HzfNQAS.jpgFSMC init as following

//--------------------------------------------------------------------------------------------------------------

port.FSMC_AddressSetupTime = 0X05;

 port.FSMC_AddressHoldTime = 0X05;

 port.FSMC_DataSetupTime =0X0c;

 port.FSMC_BusTurnAroundDuration = 0X0a;

 port.FSMC_CLKDivision = 0X00;

 port.FSMC_DataLatency = 0X19;

 port.FSMC_AccessMode = FSMC_AccessMode_A;  

FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM2;

FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Disable;

FSMC_NORSRAMInitStructure.FSMC_MemoryType =FSMC_MemoryType_SRAM;//;  FSMC_MemoryType_NOR

FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_8b;

FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode = FSMC_BurstAccessMode_Disable;

FSMC_NORSRAMInitStructure.FSMC_AsynchronousWait = FSMC_AsynchronousWait_Disable;

FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low;

FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable;

FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState;

FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable;

FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Disable;

FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Disable;

FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Disable;

FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &port;

FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &port;

FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure);

FSMC_NORSRAMCmd(FSMC_Bank1_NORSRAM2, ENABLE); 

//-----------------------------------------------------------------------------------------------------------------------------

So can you give me some direction to debug? thank you!

BRs,

JHL​

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

This is probably the interrupt being executed twice, due to late flag clear.

JW

View solution in original post

2 REPLIES 2
waclawek.jan
Super User

This is probably the interrupt being executed twice, due to late flag clear.

JW

jhl14
Associate II

Thank you, JW. You SHORT words exactly shot it. When doing the following change, the problem is gone.

//----------------------------------------------------------------------------------------------------

void TIM2_IRQHandler(void)

{

TIM_ClearITPendingBit(TIM2,TIM_IT_Update);

SPI1->DR = 0; // SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b;

FTadd = Word_Upload++; // #define FTadd (*( uint16_t *)0x64000002)

}

//----------------------------------------------------------------------------------------------------

Got the following form.0693W000006I5BEQA0.jpgthanks again and like this community!!! :D

BRs

JHL