2021-01-08 04:18 AM
Hi Team,
Basing on the lastest "STM32F4xx_StdPeriph_Driver" to Read SPI data and then write into external FSMC(8bit) device in the PWM interrupt like following .
//----------------------------------------------------------------------------------------------------
void TIM2_IRQHandler(void)
{
SPI1->DR = 0; // SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b;
FTadd = Word_Upload++; // #define FTadd (*( uint16_t *)0x64000002)
TIM_ClearITPendingBit(TIM2,TIM_IT_Update);
}
//----------------------------------------------------------------------------------------------------
But from the LA waveform below, both SPI clock and FSMC #WR ops doubled.FSMC init as following
//--------------------------------------------------------------------------------------------------------------
port.FSMC_AddressSetupTime = 0X05;
port.FSMC_AddressHoldTime = 0X05;
port.FSMC_DataSetupTime =0X0c;
port.FSMC_BusTurnAroundDuration = 0X0a;
port.FSMC_CLKDivision = 0X00;
port.FSMC_DataLatency = 0X19;
port.FSMC_AccessMode = FSMC_AccessMode_A;
FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM2;
FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Disable;
FSMC_NORSRAMInitStructure.FSMC_MemoryType =FSMC_MemoryType_SRAM;//; FSMC_MemoryType_NOR
FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_8b;
FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode = FSMC_BurstAccessMode_Disable;
FSMC_NORSRAMInitStructure.FSMC_AsynchronousWait = FSMC_AsynchronousWait_Disable;
FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low;
FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable;
FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState;
FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable;
FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Disable;
FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Disable;
FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Disable;
FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &port;
FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &port;
FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure);
FSMC_NORSRAMCmd(FSMC_Bank1_NORSRAM2, ENABLE);
//-----------------------------------------------------------------------------------------------------------------------------
So can you give me some direction to debug? thank you!
BRs,
JHL
Solved! Go to Solution.
2021-01-08 06:32 AM
This is probably the interrupt being executed twice, due to late flag clear.
JW
2021-01-08 06:32 AM
This is probably the interrupt being executed twice, due to late flag clear.
JW
2021-01-08 11:24 PM
Thank you, JW. You SHORT words exactly shot it. When doing the following change, the problem is gone.
//----------------------------------------------------------------------------------------------------
void TIM2_IRQHandler(void)
{
TIM_ClearITPendingBit(TIM2,TIM_IT_Update);
SPI1->DR = 0; // SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b;
FTadd = Word_Upload++; // #define FTadd (*( uint16_t *)0x64000002)
}
//----------------------------------------------------------------------------------------------------
Got the following form.thanks again and like this community!!!
BRs
JHL