2024-02-16 3:48 AM
Hi,
I would like to make an application to access micro sd card via SPI from STM32F407VG-DISC1 board. I have configured the pins as seen in table below.
Main file is also attached.
However, when I run the application I get FR_NO_FILESYSTEM error. My card is formatted as FAT32. It is class4 2GB micro SD card.
When I remove the SD card then I received another error that is FR_NOT_READY. So, this got me thinking that, I have made proper connections, but there is problem with the code.
Could you please point me to the right direction ?
STM32F407VG-DISC1 | HW125 SD CARD MODULE |
PC2 | MISO PIN |
PC3 | MOSI PIN |
PB10 | SCK PIN |
PB12 | GPIO_OUTPUT |
GND | GND |
5V | VCC |
Solved! Go to Solution.
2024-02-19 7:19 AM - edited 2024-02-19 7:24 AM
You have to un-mark one before you can mark a different one
Clikck on the in the top-right of the post:
Then choose 'Not the solution':
#UnmarkSolution