Skip to main content
Senior
February 16, 2024
Solved

SD Card no file system error.

Hi,

I would like to make an application to access micro sd card via SPI from STM32F407VG-DISC1 board. I have configured the pins as seen in table below.

Main file is also attached. 

However, when I run the application I get FR_NO_FILESYSTEM error. My card is formatted as FAT32. It is class4 2GB micro SD card. 

When I remove the SD card then I received another error that is FR_NOT_READY. So, this got me thinking that, I have made proper connections, but there is problem with the code.

Could you please point me to the right direction ?

 

STM32F407VG-DISC1HW125 SD CARD MODULE
PC2 MISO PIN
PC3MOSI PIN
PB10 SCK PIN
PB12 GPIO_OUTPUT
GNDGND
5VVCC



 

This topic has been closed for replies.
demirBest answer
Senior
February 19, 2024

Hi @Andrew Neil 

I came to know that SD Card needs some to settle. So, the only I have done is that, I added some delay before mountin the SD card as below. Hope it helps.

demir_0-1708351527727.png

 

 

11 replies

AScha.3
Super User
February 16, 2024

Hi,

Just a question: F407 has SDIO for sd-card access -- why you dont use it ?

 

AScha3_0-1708084970675.png

+

Keep wires to sd-card short , < 50mm is ok; long wires will make problems....

If you feel a post has answered your question, please click on " Best Answer ".
demirAuthor
Senior
February 16, 2024

Thanks Ascha.3.

This is the task actually.

Andrew Neil
Super User
February 16, 2024

@demir wrote:

When I remove the SD card then I received another error that is FR_NOT_READY. So, this got me thinking that, I have made proper connections,


Not necessarily.

The card present/not-present might just be detected on a switch ...

Have you tried tracing back to where the error is actually raised?

 


@demir wrote:

HW125 SD CARD MODULE


Do you mean one of these?

AndrewNeil_0-1708086235076.png

Do you have a link to its datasheet?


 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
demirAuthor
Senior
February 16, 2024

Thanks Andrew.

Yes, I use one of those. I searched but cant find the datasheet.

I ve debugged the code, please see the attachment. This is where code returns no file system.

Andrew Neil
Super User
February 16, 2024

If you can't find a datasheet, how can you be sure you have the correct connections?

:flushed_face:

 


@demir wrote:

This is where code returns no file system.


So step into find_volume() to find what causes it to return that error

AndrewNeil_0-1708090561676.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
demirAuthor
Senior
February 19, 2024

Cant mark it as the solution, there is no option to select.

Andrew Neil
Super User
February 19, 2024

You have to un-mark one before you can mark a different one

Clikck on the AndrewNeil_3-1708356226886.pngin the top-right of the post:

AndrewNeil_1-1708356181338.png

Then choose 'Not the solution':

AndrewNeil_0-1708356121086.png

#UnmarkSolution

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
HDaji.1
Senior
April 10, 2025

Hi @demir 

Did you figure it out this solution yourself or you follow some examples?
I only find a kind-of-official tutorial by STM staff, which, however, uses SDIO, not SPI.

 

Best