Solved
SD Card no file system error.
- 11 replies
- 6877 views
Hi,
I would like to make an application to access micro sd card via SPI from STM32F407VG-DISC1 board. I have configured the pins as seen in table below.
Main file is also attached.
However, when I run the application I get FR_NO_FILESYSTEM error. My card is formatted as FAT32. It is class4 2GB micro SD card.
When I remove the SD card then I received another error that is FR_NOT_READY. So, this got me thinking that, I have made proper connections, but there is problem with the code.
Could you please point me to the right direction ?
| STM32F407VG-DISC1 | HW125 SD CARD MODULE |
| PC2 | MISO PIN |
| PC3 | MOSI PIN |
| PB10 | SCK PIN |
| PB12 | GPIO_OUTPUT |
| GND | GND |
| 5V | VCC |