2025-03-12 11:51 AM
We have STM32F405RGT6 and we want to implement DAC through DMA.
We used an example for STM32F429ZI-Nucleo
Here is an actual code where we have an underrun the error and we need help to clarify reason and find a solution, thanks!:
#include "main.h"
#include "usb_device.h"
#include "math.h"
#define SAWTOOTH_MAX 4095 // Максимальне значення DAC (12-біт)
#define DAC_BUFFER_SIZE 100
#define PI 3.1415926
uint16_t sawtooth_value = 0; // Значення пилкоподібного сигналу
uint16_t dac_buffer[DAC_BUFFER_SIZE];
void Generate_SineWave() {
for (int i = 0; i < DAC_BUFFER_SIZE; i++) {
dac_buffer[i] = (uint16_t)(((sin(i * 2 * PI / DAC_BUFFER_SIZE) + 1) * (4096 / 2)));
}
}
#define VDDA_APPLI ((uint32_t)3300)
*/
#define DIGITAL_SCALE_12BITS (__LL_DAC_DIGITAL_SCALE(LL_DAC_RESOLUTION_12B))
#define WAVEFORM_AMPLITUDE (VDDA_APPLI)
#define WAVEFORM_FREQUENCY ((uint32_t)1000)
#define WAVEFORM_SAMPLES_SIZE (sizeof (WaveformSine_12bits_32samples) / sizeof (uint16_t))
#define WAVEFORM_TIMER_FREQUENCY (WAVEFORM_FREQUENCY * WAVEFORM_SAMPLE_SIZE)
#define WAVEFORM_TIMER_FREQUENCY_RANGE_MIN ((uint32_t) 1)
#define WAVEFORM_TIMER_PRESCALER_MAX_VALUE ((uint32_t)0xFFFF-1)
#define __WAVEFORM_AMPLITUDE_SCALING(__DATA_12BITS__) \
(__DATA_12BITS__ \
* __LL_DAC_CALC_VOLTAGE_TO_DATA(VDDA_APPLI, WAVEFORM_AMPLITUDE, LL_DAC_RESOLUTION_12B) \
/ __LL_DAC_DIGITAL_SCALE(LL_DAC_RESOLUTION_12B) \
)
const uint16_t WaveformSine_12bits_32samples[] =
{
__WAVEFORM_AMPLITUDE_SCALING(2048),
__WAVEFORM_AMPLITUDE_SCALING(2447),
__WAVEFORM_AMPLITUDE_SCALING(2831),
__WAVEFORM_AMPLITUDE_SCALING(3185),
__WAVEFORM_AMPLITUDE_SCALING(3495),
__WAVEFORM_AMPLITUDE_SCALING(3750),
__WAVEFORM_AMPLITUDE_SCALING(3939),
__WAVEFORM_AMPLITUDE_SCALING(4056),
__WAVEFORM_AMPLITUDE_SCALING(4095),
__WAVEFORM_AMPLITUDE_SCALING(4056),
__WAVEFORM_AMPLITUDE_SCALING(3939),
__WAVEFORM_AMPLITUDE_SCALING(3750),
__WAVEFORM_AMPLITUDE_SCALING(3495),
__WAVEFORM_AMPLITUDE_SCALING(3185),
__WAVEFORM_AMPLITUDE_SCALING(2831),
__WAVEFORM_AMPLITUDE_SCALING(2447),
__WAVEFORM_AMPLITUDE_SCALING(2048),
__WAVEFORM_AMPLITUDE_SCALING(1649),
__WAVEFORM_AMPLITUDE_SCALING(1265),
__WAVEFORM_AMPLITUDE_SCALING(911),
__WAVEFORM_AMPLITUDE_SCALING(601),
__WAVEFORM_AMPLITUDE_SCALING(346),
__WAVEFORM_AMPLITUDE_SCALING(157),
__WAVEFORM_AMPLITUDE_SCALING(40),
__WAVEFORM_AMPLITUDE_SCALING(0),
__WAVEFORM_AMPLITUDE_SCALING(40),
__WAVEFORM_AMPLITUDE_SCALING(157),
__WAVEFORM_AMPLITUDE_SCALING(346),
__WAVEFORM_AMPLITUDE_SCALING(601),
__WAVEFORM_AMPLITUDE_SCALING(911),
__WAVEFORM_AMPLITUDE_SCALING(1265),
__WAVEFORM_AMPLITUDE_SCALING(1649)
};
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_DAC_Init(void);
static void MX_TIM6_Init(void);
void LED_Init(void);
void Configure_DMA(void);
void Configure_TIM_TimeBase_DAC_trigger(void);
void Configure_DAC(void);
void Activate_DAC(void);
void LED_Blinking(uint32_t Period);
void Debug_GPIO_Init(void);
void Debug_LED_Blink(uint32_t count, uint32_t period);
void Debug_Check_Timers(void);
void Debug_Check_DMA(void);
void Debug_Check_DAC(void);
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
// MX_DMA_Init();
// MX_USB_DEVICE_Init();
// MX_DAC_Init();
// MX_TIM6_Init();
Generate_SineWave();
LED_Init();
Configure_DMA();
Configure_TIM_TimeBase_DAC_trigger();
Configure_DAC();
Activate_DAC();
while (1)
{
}
}
void LED_Init(void)
{
LED1_GPIO_CLK_ENABLE();
LL_GPIO_SetPinMode(LED1_GPIO_PORT, LED1_PIN, LL_GPIO_MODE_OUTPUT);
//LL_GPIO_SetPinOutputType(LED1_GPIO_PORT, LED1_PIN, LL_GPIO_OUTPUT_PUSHPULL);
//LL_GPIO_SetPinSpeed(LED1_GPIO_PORT, LED1_PIN, LL_GPIO_SPEED_FREQ_LOW);
//LL_GPIO_SetPinPull(LED1_GPIO_PORT, LED1_PIN, LL_GPIO_PULL_NO);
}
void Configure_DMA(void)
{
NVIC_SetPriority(DMA1_Stream5_IRQn, 1); /* DMA IRQ lower priority than DAC IRQ */
NVIC_EnableIRQ(DMA1_Stream5_IRQn);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1);
LL_DMA_SetChannelSelection(DMA1, LL_DMA_STREAM_5, LL_DMA_CHANNEL_7);
LL_DMA_ConfigTransfer(DMA1, LL_DMA_MODE_CIRCULAR);
LL_DMA_ConfigAddresses(DMA1,
LL_DMA_STREAM_5,
(uint32_t)&WaveformSine_12bits_32samples,
LL_DAC_DMA_GetRegAddr(DAC1, LL_DAC_CHANNEL_1, LL_DAC_DMA_REG_DATA_12BITS_RIGHT_ALIGNED),
LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
LL_DMA_SetDataLength(DMA1,
LL_DMA_STREAM_5,
WAVEFORM_SAMPLES_SIZE);
LL_DMA_EnableIT_TE(DMA1,
LL_DMA_STREAM_5);
LL_DMA_EnableStream(DMA1,
LL_DMA_STREAM_5);
}
void Configure_TIM_TimeBase_DAC_trigger(void)
{
uint32_t timer_clock_frequency = 0; /* Timer clock frequency */
uint32_t timer_prescaler = 0; /* Time base prescaler to have timebase aligned on minimum frequency possible */
uint32_t timer_reload = 0; /* Timer reload value in function of timer prescaler to achieve time base period */
if (LL_RCC_GetAPB1Prescaler() == LL_RCC_APB1_DIV_1)
{
timer_clock_frequency = __LL_RCC_CALC_PCLK1_FREQ(SystemCoreClock, LL_RCC_GetAPB1Prescaler());
}
else
{
timer_clock_frequency = (__LL_RCC_CALC_PCLK1_FREQ(SystemCoreClock, LL_RCC_GetAPB1Prescaler()) * 2);
}
timer_prescaler = ((timer_clock_frequency / (WAVEFORM_TIMER_PRESCALER_MAX_VALUE * WAVEFORM_TIMER_FREQUENCY_RANGE_MIN)) +1);
timer_reload = (timer_clock_frequency / (timer_prescaler * WAVEFORM_TIMER_FREQUENCY));
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_TIM6);
LL_TIM_SetPrescaler(TIM6, (timer_prescaler - 1));
LL_TIM_SetAutoReload(TIM6, (timer_reload - 1));//83
LL_TIM_SetCounterMode(TIM6, LL_TIM_COUNTERMODE_UP);
LL_TIM_SetTriggerOutput(TIM6, LL_TIM_TRGO_UPDATE);
LL_TIM_EnableCounter(TIM6);
}
void Configure_DAC(void)
{
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOA);
LL_GPIO_SetPinMode(GPIOA, LL_GPIO_PIN_4, LL_GPIO_MODE_ANALOG);
NVIC_SetPriority(TIM6_DAC_IRQn, 0);
NVIC_EnableIRQ(TIM6_DAC_IRQn);
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_DAC1);
// LL_DAC_SetMode(DAC1, LL_DAC_CHANNEL_1, LL_DAC_MODE_NORMAL_OPERATION);
LL_DAC_SetTriggerSource(DAC1, LL_DAC_CHANNEL_1, LL_DAC_TRIG_EXT_TIM6_TRGO);
//LL_DAC_SetOutputBuffer(DAC1, LL_DAC_CHANNEL_1, LL_DAC_OUTPUT_BUFFER_ENABLE);
LL_DAC_EnableDMAReq(DAC1, LL_DAC_CHANNEL_1);
LL_DAC_EnableIT_DMAUDR1(DAC1);
}
void Activate_DAC(void)
{
__IO uint32_t wait_loop_index = 0;
LL_DAC_Enable(DAC1, LL_DAC_CHANNEL_1);
HAL_Delay(1000);
wait_loop_index = ((LL_DAC_DELAY_STARTUP_VOLTAGE_SETTLING_US * (SystemCoreClock / (100000 * 2))) / 10);
while(wait_loop_index != 0)
{
wait_loop_index--;
}
LL_DAC_EnableTrigger(DAC1, LL_DAC_CHANNEL_1);
}
void SystemClock_Config(void)
{
LL_FLASH_SetLatency(LL_FLASH_LATENCY_5);
while(LL_FLASH_GetLatency()!= LL_FLASH_LATENCY_5)
{
}
LL_PWR_SetRegulVoltageScaling(LL_PWR_REGU_VOLTAGE_SCALE1);
LL_RCC_HSE_Enable();
while(LL_RCC_HSE_IsReady() != 1)
{
}
LL_RCC_PLL_ConfigDomain_SYS(LL_RCC_PLLSOURCE_HSE, LL_RCC_PLLM_DIV_4, 168, LL_RCC_PLLP_DIV_2);
LL_RCC_PLL_ConfigDomain_48M(LL_RCC_PLLSOURCE_HSE, LL_RCC_PLLM_DIV_4, 168, LL_RCC_PLLQ_DIV_7);
LL_RCC_PLL_Enable();
while(LL_RCC_PLL_IsReady() != 1)
{
}
while (LL_PWR_IsActiveFlag_VOS() == 0)
{
}
LL_RCC_SetAHBPrescaler(LL_RCC_SYSCLK_DIV_1);
LL_RCC_SetAPB1Prescaler(LL_RCC_APB1_DIV_4);
LL_RCC_SetAPB2Prescaler(LL_RCC_APB2_DIV_2);
LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_PLL);
while(LL_RCC_GetSysClkSource() != LL_RCC_SYS_CLKSOURCE_STATUS_PLL)
{
}
LL_SetSystemCoreClock(168000000);
if (HAL_InitTick (TICK_INT_PRIORITY) != HAL_OK)
{
Error_Handler();
}
}
static void MX_DAC_Init(void)
{
LL_DAC_InitTypeDef DAC_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_DAC1);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOA);
GPIO_InitStruct.Pin = LL_GPIO_PIN_4;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
LL_DMA_SetChannelSelection(DMA1, LL_DMA_STREAM_5, LL_DMA_CHANNEL_7);
LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_STREAM_5, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
LL_DMA_SetStreamPriorityLevel(DMA1, LL_DMA_STREAM_5, LL_DMA_PRIORITY_VERYHIGH);
LL_DMA_SetMode(DMA1, LL_DMA_STREAM_5, LL_DMA_MODE_CIRCULAR);
LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_STREAM_5, LL_DMA_PERIPH_NOINCREMENT);
LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_STREAM_5, LL_DMA_MEMORY_INCREMENT);
LL_DMA_SetPeriphSize(DMA1, LL_DMA_STREAM_5, LL_DMA_PDATAALIGN_WORD);
LL_DMA_SetMemorySize(DMA1, LL_DMA_STREAM_5, LL_DMA_MDATAALIGN_WORD);
LL_DMA_EnableFifoMode(DMA1, LL_DMA_STREAM_5);
LL_DMA_SetFIFOThreshold(DMA1, LL_DMA_STREAM_5, LL_DMA_FIFOTHRESHOLD_FULL);
LL_DMA_SetMemoryBurstxfer(DMA1, LL_DMA_STREAM_5, LL_DMA_MBURST_SINGLE);
LL_DMA_SetPeriphBurstxfer(DMA1, LL_DMA_STREAM_5, LL_DMA_PBURST_SINGLE);
NVIC_SetPriority(TIM6_DAC_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
NVIC_EnableIRQ(TIM6_DAC_IRQn);
DAC_InitStruct.TriggerSource = LL_DAC_TRIG_EXT_TIM6_TRGO;
DAC_InitStruct.WaveAutoGeneration = LL_DAC_WAVE_AUTO_GENERATION_NONE;
DAC_InitStruct.OutputBuffer = LL_DAC_OUTPUT_BUFFER_ENABLE;
LL_DAC_Init(DAC, LL_DAC_CHANNEL_1, &DAC_InitStruct);
}
static void MX_TIM6_Init(void)
{
LL_TIM_InitTypeDef TIM_InitStruct = {0};
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_TIM6);
NVIC_SetPriority(TIM6_DAC_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
NVIC_EnableIRQ(TIM6_DAC_IRQn);
TIM_InitStruct.Prescaler = 0;
TIM_InitStruct.CounterMode = LL_TIM_COUNTERMODE_UP;
TIM_InitStruct.Autoreload = 1;
LL_TIM_Init(TIM6, &TIM_InitStruct);
LL_TIM_DisableARRPreload(TIM6);
LL_TIM_SetTriggerOutput(TIM6, LL_TIM_TRGO_RESET);
LL_TIM_DisableMasterSlaveMode(TIM6);
}
static void MX_DMA_Init(void)
{
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1);
NVIC_SetPriority(DMA1_Stream5_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
NVIC_EnableIRQ(DMA1_Stream5_IRQn);
}
static void MX_GPIO_Init(void)
{
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOH);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOA);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOB);
LL_GPIO_ResetOutputPin(LED_GPIO_Port, LED_Pin);
GPIO_InitStruct.Pin = LED_Pin;
GPIO_InitStruct.Mode = LL_GPIO_MODE_OUTPUT;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(LED_GPIO_Port, &GPIO_InitStruct);
}
void DacDmaTransferError_Callback()
{
LED_Blinking(LED_BLINK_ERROR);
}
void DacUnderrunError_Callback(void)
{
LL_DAC_DisableIT_DMAUDR1(DAC1);
LED_Blinking(LED_BLINK_ERROR);
}
void LED_Blinking(uint32_t Period)
{
LL_GPIO_SetOutputPin(LED1_GPIO_PORT, LED1_PIN);
while (1)
{
LL_GPIO_TogglePin(LED1_GPIO_PORT, LED1_PIN);
LL_mDelay(Period);
}
}
void Debug_LED_Blink(uint32_t count, uint32_t period)
{
for (uint32_t i = 0; i < count; i++)
{
LL_GPIO_TogglePin(GPIOB, LL_GPIO_PIN_2);
LL_mDelay(period);
}
}
void Debug_Check_Timers(void)
{
if (!LL_TIM_IsEnabledCounter(TIM6))
{
Debug_LED_Blink(3, 200);
}
}
void Debug_Check_DMA(void)
{
if (!LL_DMA_IsEnabledStream(DMA1, LL_DMA_STREAM_5))
{
Debug_LED_Blink(2, 500);
}
}
void Debug_Check_DAC(void)
{
if (!LL_DAC_IsEnabled(DAC1, LL_DAC_CHANNEL_1))
{
Debug_LED_Blink(5, 100);
}
}
void Error_Handler(void)
{
__disable_irq();
while (1)
{
}
}
#ifdef USE_FULL_ASSERT
void assert_failed(uint8_t *file, uint32_t line)
{
}
#endif /* USE_FULL_ASSERT */
stm32f4xx_it.c:
#include "main.h"
#include "stm32f4xx_it.h"
extern PCD_HandleTypeDef hpcd_USB_OTG_FS;
void NMI_Handler(void)
{
while (1)
{
}
}
void HardFault_Handler(void)
{
while (1)
{
}
}
void MemManage_Handler(void)
{
while (1)
{
}
}
void BusFault_Handler(void)
{
while (1)
{
}
}
void UsageFault_Handler(void)
{
while (1)
{
}
}
void SVC_Handler(void)
{
}
void DebugMon_Handler(void)
{
}
void PendSV_Handler(void)
{
}
void SysTick_Handler(void)
{
HAL_IncTick();
}
void DMA1_Stream5_IRQHandler(void)
{
/* USER CODE BEGIN DMA1_Stream5_IRQn 0 */
/* Check whether DMA transfer error caused the DMA interruption */
if(LL_DMA_IsActiveFlag_TE7(DMA1) == 1)
{
/* Clear flag DMA transfer error */
LL_DMA_ClearFlag_TE7(DMA1);
/* Call interruption treatment function */
DacDmaTransferError_Callback();
}
/* USER CODE END DMA1_Stream5_IRQn 0 */
}
void TIM6_DAC_IRQHandler(void)
{
// if (LL_TIM_IsActiveFlag_UPDATE(TIM6)) {
// Debug_LED_Blink(100, 100);
// LL_TIM_ClearFlag_UPDATE(TIM6);
// }
/* USER CODE BEGIN TIM6_DAC_IRQn 0 */
/* Check whether DAC channel1 underrun caused the DAC interruption */
if(LL_DAC_IsActiveFlag_DMAUDR1(DAC1) != 0)
{
if (LL_DMA_GetDataLength(DMA1, LL_DMA_STREAM_5) == 0)
{
Debug_LED_Blink(3, 200); // Blinks 3 times if DMA is not transferring data
}
if (!LL_TIM_IsEnabledCounter(TIM6)) {
Debug_LED_Blink(4, 300);
}
if (LL_TIM_GetCounter(TIM6) == 0)
{
Debug_LED_Blink(4, 300); // Blinks 4 times if TIM6 is not counting
}
if (!LL_DAC_IsEnabled(DAC1, LL_DAC_CHANNEL_1))
{
Debug_LED_Blink(5, 100); // Blinks 5 times if DAC is not enabled
}
if (LL_DMA_GetDataLength(DMA1, LL_DMA_STREAM_5) == 0)
{
Debug_LED_Blink(3, 200); // DMA not transferring
}
Debug_Check_Timers();
Debug_Check_DMA();
Debug_Check_DAC();
/* Clear flag DAC channel1 underrun */
LL_DAC_ClearFlag_DMAUDR1(DAC1);
/* Call interruption treatment function */
DacUnderrunError_Callback();
}
/* USER CODE END TIM6_DAC_IRQn 0 */
/* USER CODE BEGIN TIM6_DAC_IRQn 1 */
/* USER CODE END TIM6_DAC_IRQn 1 */
}
void OTG_FS_IRQHandler(void)
{
HAL_PCD_IRQHandler(&hpcd_USB_OTG_FS);
}
2025-03-12 11:52 AM