2020-06-04 05:02 AM
I make a big project with F439 MCU and there are many things on the board like WiFi, BT, EEPROM, Flash, GPS and so on. The latest thing I made was activating ETH and it works good at least ping runs perfect. But later I found that the USB OTG HS CDC which worked perfectly now doesn't work. Win10 can not recognize the USB divice and Terminal programm can not connect to the port (port is visible some how), firmware freezing. I appreciate any suggestions.
2020-06-04 05:49 AM
> firmware freezing
Maybe investigate where/why that's happening.
2020-06-04 07:35 AM
2020-06-04 08:09 AM
2020-06-05 01:00 AM
Many thanks TDK. I played around with HEAp and STACK sizes but had no reaction from freezing. Than I have defined which "something" got access beyond the RAM. I forgot to limit wifi data massive which gets the data by IRQ. Result is HardFault.
2020-06-10 04:32 PM